Skip to main content
JAitc.1
Associate II
October 31, 2022
Question

How to Reset STM32 Timer Internal Trigger Connections

I'm using the STM32H735 to create a sequence of PWM signals. I have timers TIM1, TIM2, TIM4, and TIM24 all connected in a slave timer chain. TIM1 triggers TIM2 with ITR0. TIM2 triggers TIM4 with ITR1, and TIM4 triggers TIM24 with ITR3. Each link in the trigger chain is done with a timer channel in "Output Compare no Output" mode setup as the TRGO event.  These are the slave modes in the chain:

TIM1: disable

TIM2:  Trigger Mode (ITR0)

TIM4:  Trigger Mode (ITR1)

TIM24:  Trigger Mode (ITR3)

This all works perfectly but only the first time. If I stop all 4 timers and try to restart the sequence, only the PWM output from TIM1 starts again. The PWM output from TIM2, TIM4 and TIM24 fails to start. 

Here is some pseudo code to show what I have.

The sequence is started with:

// TIMER 24

HAL_TIM_Base_Start(&htim24);

HAL_TIM_PWM_Start(&htim24, TIM_CHANNEL_4);

// TIMER 4

HAL_TIM_Base_Start(&htim4);

HAL_TIM_PWM_Start(&htim4, TIM_CHANNEL_3);

HAL_TIM_OC_Start(&htim4, TIM_CHANNEL_2);

// TIMER 2

HAL_TIM_Base_Start(&htim2);

HAL_TIM_OC_Start(&htim2, TIM_CHANNEL_3);

HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_4);

// TIMER 1

HAL_TIM_Base_Start(&htim1);

HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);

HAL_TIM_OC_Start(&htim1, TIM_CHANNEL_2);

The sequence is then stopped with:

// TIMER 1

HAL_TIM_Base_Stop(&htim1);

HAL_TIM_PWM_Stop(&htim1, TIM_CHANNEL_1);

HAL_TIM_OC_Stop(&htim1, TIM_CHANNEL_2);

// TIMER 2

HAL_TIM_Base_Stop(&htim2);

HAL_TIM_OC_Stop(&htim2, TIM_CHANNEL_3);

HAL_TIM_PWM_Stop(&htim2, TIM_CHANNEL_4);

// TIMER 4

HAL_TIM_Base_Stop(&htim4);

HAL_TIM_PWM_Stop(&htim4, TIM_CHANNEL_3);

HAL_TIM_OC_Stop(&htim4, TIM_CHANNEL_2);

// TIMER 24

HAL_TIM_Base_Stop(&htim24);

HAL_TIM_PWM_Stop(&htim24, TIM_CHANNEL_4);

After the stop code the all 4 PWM signals stop. When the start code is run again, only TIM1_CH1 has PWM output. I suspect there needs to be a manual reset of the Internal Trigger connections for TIM2, TIM4 and TIM24 but I don't see anything for this in the HAL. Does anyone know what's required to reset the timers in this situation? Thanks in advance.

This topic has been closed for replies.

12 replies

JAitc.1
JAitc.1Author
Associate II
November 1, 2022

Just to clarify: When I say "only the first time" I mean, when timer start code is run the first time, all 4 PWM outputs keep running correctly until the timer stop code is run. The problem occurs when the timer start code is then run a second time.

ypkdani
Associate
April 15, 2023

Hello,

did you find a solution? i have the same problem

waclawek.jan
Super User
April 15, 2023

Read out the timers' registers, first in working, then in non-working state, and check/compare/post.

JW

aasil
Associate
November 7, 2023

i have same problem when stop pwm and start again slave timer has 100% Duty cycle, do you find a solution?

Associate
January 23, 2024

Hello !

I had the same problem when I want to generate two PWM signals shifted by an adjustable delay. I found the answer in this part of the reference manual of the STM32H723/733, STM32H725/735 "43.3.10 Output compare mode". In this part, I have seen :

"The output pin can keep its level (OCXM=0000), be set active (OCxM=0001), be set inactive (OCxM=0010) or can toggle (OCxM=0011) on match."

In my project, made with CubeMX, I have set up "active level on match", but it must be "toggle on match" (TIM_OCMODE_TOGGLE in code for sConfigOC.OCMode).

My hypothesis is that on the first capture of the OC2REF for the slave timer, the output pin stays always high so when we restart the timer we cannot trigger, because the signal is high. I'm not sure if it is the correct understanding, but it works for me :)

Regards.

Explorer II
November 24, 2024

@Cruvix your solution works great, but I still don't understand why? can someone assist with the answer?

waclawek.jan
Super User
November 24, 2024

The answer is already there: the trigger in slave-mode controller works on edge. If in the master you don't generate an edge, there's no trigger.

JW

Explorer II
November 24, 2024

Given that

  1. Timer 2 is configured as Active Level On Match, and
  2. I use the HAL_TIM_PWM_Stop() function on the master as well

Then why wouldn't the HAL_TIM_PWM_Start() re-initialize the trigger? And why would the Toggle On Match setting does?

Please excuse my rudimentary line of questioning, kindly advise.

waclawek.jan
Super User
November 24, 2024

I don't use Cube/HAL, but it's open source, so you can simply observe the timers' registers while stepping through those functions.

If you are not sure what the registers contents mean, post them here (together with those changes).

JW

Explorer II
November 25, 2024

Dear@waclawek.jan ,

First of all, thank you for taking the time to answer my questions, I sincerely appreciate it.

Secondly, my question is not regarding the usage of HALs, but more of a function question - getting my head around the resetting of the OCxREF signal when set to "active level on match":

If I were to set "active level on match" for a certain timer's output compare channel, then I would expect that upon stopping the timer there should be a way to reset the OCxREF signal, but I couldn't find any. Can you advise on the proper way to reset the timer so that when I reactivate it the next time, the OCxREF signal will generate a positive edge on match again?

Thanks again for the help,

BA

waclawek.jan
Super User
November 25, 2024

In microcontrollers, there's never one single "proper" way to do things; everything is context-dependent and there are myriads of combinations of circumstances and settings.

One way to clear OCxREF is to set TIMx.CCMRx.OCxM=0b100 for Force inactive level.

(A nice exercise for this is to write the basic loopdelay blinky by replacing GPIO Out toggling by alternately setting a TIMx_CHx pin using the Force Inactive and Force Active).

JW

Explorer II
November 28, 2024

Thank you for the assistance @waclawek.jan , going to Force Inactive Level and then going back to Active On Match solved the entire issue.

Another thing that I have noticed is that if I want to maintain the synchronization between channels, then I would have to force an update by setting the UG flag prior to reinitializing the timers.

Thanks again!

BA