Skip to main content
anran99
Associate II
May 26, 2008
Question

How to remap PD0/PD1 for STM32101C8 ?

  • May 26, 2008
  • 6 replies
  • 1574 views
Posted on May 26, 2008 at 17:34

How to remap PD0/PD1 for STM32101C8 ?

    This topic has been closed for replies.

    6 replies

    anran99
    anran99Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:35

    thx, but It's STM32101C8 . PD0/PD1 remap on OSC_IN and OSC_OUT pin.

    I can't set the PD0/PD1 as output mode !

    Maybe this is a bug ,I couldn't resolved it .

    I need a demo sourcecode to remap .

    appreciate your help .:D

    julien
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:35

    I suppose that you want to remap the CAN on the GPIO D0/D1

    //CAN Remappper sur D0 et D1

    GPIO_PinRemapConfig(GPIO_Remap2_CAN, ENABLE);

    /* Configure CAN pin: RX */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_Init(GPIOD, &GPIO_InitStructure);

    /* Configure CAN pin: TX */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

    GPIO_Init(GPIOD, &GPIO_InitStructure);

    [ This message was edited by: julien.massot on 14-05-2008 14:28 ]

    anran99
    anran99Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:35

    Pls give a correct example, I can't post my code.

    [ This message was edited by: anran99 on 14-05-2008 07:07 ]

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:35

    Hi,

    Check our last documents on web RM0008 version 4 and Erratasheet version 3 ( May 2008) Let me know if you get more questions on this.

    Cheers,

    STOne-32.

    jj_it
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:35

    Hi - am awaiting new board run - perhaps this suggestion may help:

    Can't find obvious error in your listing. Would like you to move this

    code to two other ''shared pins'' - and see IF the inability to set as

    output persists. In this manner you - at least - will see if the problem is PD0/PD1 specific. Again - you must comb your part's pin-outs to find suitable (those which aren't ''natually'' I/O) pins to ''re-map.''

    anran99
    anran99Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:35

    my test code :

    /**********************************************************************/

    void RCC_Configuration(void)

    {

    /* RCC system reset(for debug purpose) */

    RCC_DeInit();

    /* Enable Prefetch Buffer */

    FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

    /* Flash 2 wait state */

    FLASH_SetLatency(FLASH_Latency_2);

    /* HCLK = SYSCLK */

    RCC_HCLKConfig(RCC_SYSCLK_Div1);

    /* PCLK2 = HCLK */

    RCC_PCLK2Config(RCC_HCLK_Div1);

    /* PCLK1 = HCLK/2 */

    RCC_PCLK1Config(RCC_HCLK_Div2);

    /* PLLCLK = 8MHz * 9 = 72 MHz */

    RCC_PLLConfig(RCC_PLLSource_HSI_Div2, RCC_PLLMul_12);

    /* Enable PLL */

    RCC_PLLCmd(ENABLE);

    /* Wait till PLL is ready */

    while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)

    {

    }

    /* Select PLL as system clock source */

    RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

    /* Wait till PLL is used as system clock source */

    while(RCC_GetSYSCLKSource() != 0x08)

    {

    }

    }

    }

    int main()

    {

    /* Configure the system clocks */

    RCC_Configuration();

    /* NVIC Configuration */

    NVIC_Configuration();

    /* Enable SWJ , Disable JTAG */

    GPIO_PinRemapConfig( GPIO_Remap_SWJ_JTAGDisable , ENABLE );

    /* AFIO Periperal Clock Enable */

    RCC_APB2PeriphClockCmd( RCC_APB2Periph_AFIO,ENABLE );

    /* Enable GPIO clock */

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD, ENABLE);

    GPIO_PinRemapConfig( GPIO_Remap_PD01 , ENABLE );

    /* Configure PD.0, PD.1 as Output push-pull */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 ;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

    GPIO_Init(GPIOD, &GPIO_InitStructure);

    // while (1)

    // {

    // GPIO_SetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

    // GPIO_ResetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

    // GPIO_SetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

    // GPIO_ResetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

    // GPIO_SetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

    // GPIO_ResetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

    // }

    }