How to reduce Data loss on Ping test on STM32F407?
We are facing data loss issue while ping test was conducted on the STM32F407 with lwip stack 1.4.1
The stack was downloaded for STM32F407 Evaluation Board Code from www.st.com site after changing pin configuration [used tftpserver standalone code] flashed into STM32f407ZE controller found that 10% of data loss.
Details:
code version on ST : STM32F4x7_ETH_LwIP_V1.1.1
Ethernet Mode used : MII Mode
Ethernet PHY : DP83848_PHY
IP : Static IP is used[DHCP mode is disabled].
tested in Both polling and interrupt method , both have same result. also tested by connecting PC Directly With Stm32407ZE target Board
note : we are not using Ethernet Link Status interrupt.