Skip to main content
Associate II
Sep 13, 2025 8:17 AM UTC
Solved

How to recover a bricked Flash STM32H743XI after accidentally pulled the RESET line while flashing a FW

Hello Community

For some reason, my post from yesterday did not go through and was marked as spam. I'm not interested in moaning about it right now, as I have managed to brick my custom board, designed with STM32H743XI and would be more interested in finding a way to unbrick it.

Before jumping to any conclusion, please read the post as it contains crucial info and things I have already tried, which you would like to suggest.

Some info about my setup, as mentioned earlier, it's a custom board with BOOT0 and RESET pins exposed using a switch, and there is a JTAG interface for debugging purposes, along with a SEGGER JLink. The way I managed to brick is that I accidentally pulled the RESET line while flashing a FW using Jlink, and since then, it seems memory is in locked mode, and neither Jlink nor ST-vLink is helpful in the rescue mission.

Things I have already tried and did not work... maybe I am missing something.

  1. I have been in this situation before, and was able to recover from it using JLInk STM32 Unlock tool, but surprisingly, this time, that too is unable to reset the Option Bytes and fails to recover.
  2. Tried using the JLink Commander tool too, which was also not able to erase the memory, returned error code -5.
  3. Tried to use STM32CubeProgrammer with Jlink, and tried to gain control of the MCU in reset mode, and tried to mass erase and reset option bytes, but it did not work.
  4. Tried to use STM32CubeProgrammer with Jlink, and tried to gain control of the MCU in reset mode using DFU by pulling BOOT0, then RESET and releasing RESET while still holding BOOT0 high and later releasing it, but that too failed to mass erase and reset option bytes.
  5. Steps 3 and 4 were also repeated using ST-vLink, but failed in the same manner.

Right now, it feels like I am running out of options to recover from this situation. If someone can point me to any other solution or point out a mistake in what I have tried out so far, I would really appreciate the help!

 

PS: My other post on the same point, which is marked down as spam, had all the screenshots for reference to what I have tried so far, and I will try to upload them here if I can.

_JJ_Best answer
Associate II
Oct 6, 2025 12:26 PM UTC

Guess what fellas, following solution worked and STM32H743Xi is back in action again.

Run JLinkSTM32.exe to unlock the device.

The default location of this file is here: C:\Program Files\SEGGER\JLink_V796e.

This can be installed from here: https://www.segger.com/downloads/jlink/ and you need to use a jlink to do this.

 

PS: Funnily enough, I was using latest from the location, which was unable to unbrick it, but one of my collegue had an older version on his system and he tried and it worked like a charm!

 

Thank you guys for all your support! Much Appreciated!

BR, JJ

34 replies

_JJ_AuthorBest answer
Associate II
Oct 6, 2025 12:26 PM UTC

Guess what fellas, following solution worked and STM32H743Xi is back in action again.

Run JLinkSTM32.exe to unlock the device.

The default location of this file is here: C:\Program Files\SEGGER\JLink_V796e.

This can be installed from here: https://www.segger.com/downloads/jlink/ and you need to use a jlink to do this.

 

PS: Funnily enough, I was using latest from the location, which was unable to unbrick it, but one of my collegue had an older version on his system and he tried and it worked like a charm!

 

Thank you guys for all your support! Much Appreciated!

BR, JJ
_JJ_Author
Associate II
Jun 9, 2026 12:39 PM UTC

Just an update, had another board in bricked state. Just running the utility as I have mentioned did not work this time.

Then I remember I used to do back in time like 5 years ago; holding the nRST# or RESET pin of the MCU while running  JLinkSTM32.exe to release the MCU from protection mode.

Publishing this supplementary info in case someone else is having same problem and above solution did not work for them.

 

Good luck! Happy debugging!

 

BR, JJ