Skip to main content
Michel Keijzers
Associate II
May 25, 2018 11:45 AM UTC
Solved

How to receive bytes from SPI with interrupts using HAL?

Posted on May 25, 2018 at 13:45

Background

(note I asked this question too at

https://electronics.stackexchange.com/questions/376282/how-to-receive-bytes-from-spi-with-interrupts-using-hal-on-stm32

, but no answers yet).

I am trying to make a SPI connection between two STM32F103C8T6's.

Measurements

According to my logic analyzer I get a signal that looks ok (sending 10 bytes with values 0x55):

Results

My receiver's callback function for RX Complete also stops in the breakpoint (last line in code below):

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)

{

/* Prevent unused argument(s) compilation warning */

if (hspi1.RxXferCount == 10)

Problem

I sent 10 bytes, however, the RxXferCount has value 0. Instead, RxXferSize has value 10, but pRxBuffPtr is empty.

Question

How can I receive the correct bytes?

**Values from the register SPI1 and variable hspi1**

https://i.stack.imgur.com/xb5X5.png

Relevant code

Initialization (using a GPIO for defining Master and Slave):

/* SPI1 init function */

static void MX_SPI1_Init(void)

{

hspi1.Instance = SPI1;

hspi1.Init.Mode = (HAL_GPIO_ReadPin(GPIOB, GPIO_PIN_12) == GPIO_PIN_SET ?

SPI_MODE_MASTER : SPI_MODE_SLAVE);

hspi1.Init.Direction = SPI_DIRECTION_2LINES;

hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

hspi1.Init.NSS = SPI_NSS_SOFT;

hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;

hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

hspi1.Init.TIMode = SPI_TIMODE_DISABLE;

hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

hspi1.Init.CRCPolynomial = 10;

if (HAL_SPI_Init(&hspi1) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

}

Main function:

int main(void)

{

...

MX_SPI1_Init();

...

_transmitter = (HAL_GPIO_ReadPin(GPIOB, GPIO_PIN_12) == GPIO_PIN_SET ?

SPI_MODE_MASTER : SPI_MODE_SLAVE);

while (1)

{

if (_transmitter)

{

uint8_t data[] = { 0x55, 0x55, 0x55, 0x55, 0x55,

0x55, 0x55, 0x55, 0x55, 0x55 };

HAL_SPI_Transmit_IT(&hspi1, data, 10);

}

else

{

HAL_SPI_Receive_IT(&hspi1, _spi_data, 10);

}

}

}

    This topic has been closed for replies.
    Michel Keijzers
    Michel KeijzersBest answer
    Associate II
    May 27, 2018 10:46 AM UTC
    Posted on May 27, 2018 at 12:46

     The problem has been 'solved'... Or better said, there was no problem in the first place. I expected the results (received data) to be in the variable 

    hspi in the interrupt handler, however, it is directly stored in the variable 

    _spi_data (passed during the receive call). And hspi is cleared up already while in the interrupt handler.

    @T J I saw your comment has been removed; thanks for your reaction though.

    1 reply

    Michel Keijzers
    Michel KeijzersAuthorBest answer
    Associate II
    May 27, 2018 10:46 AM UTC
    Posted on May 27, 2018 at 12:46

     The problem has been 'solved'... Or better said, there was no problem in the first place. I expected the results (received data) to be in the variable 

    hspi in the interrupt handler, however, it is directly stored in the variable 

    _spi_data (passed during the receive call). And hspi is cleared up already while in the interrupt handler.

    @T J I saw your comment has been removed; thanks for your reaction though.