Skip to main content
Associate
Feb 22, 2024 10:40 PM UTC
Question

How to read data from a sensor

So, I'm trying to read data from a dht11 sensor.

 

In the datasheet says that you have to send high signal, wait 80ms, then low signal, and dht11 will start sending data.

My problem is, I don't know how to debug this. I don't know how to see if I my sensor is sending me data. How can I see this using STM32Cube IDE?

This topic has been closed for replies.

6 replies

Lead II
Feb 23, 2024 5:14 AM UTC

Arduino - DHT11 | Arduino Tutorial (arduinogetstarted.com)

Overview | DHT11, DHT22 and AM2302 Sensors | Adafruit Learning System

DHT11 Humidity & Temperature Sensor (mouser.com)

I think, you mean 80 micro-sec (not ms as milli-sec)?

As I understand this chip:

  • you have to change all the time the direction
  • it looks a bit like a "single wire interface": some MCUs have support for such an interface
  • if you want to do with "bit-banging" (in GPIO mode): it changes all the time the direction: MCU ties pin down, and starts to read.
    Luckily: it seems to be an Open Drain logic (with a pull-up): just configure as Open Drain output (just to tie low via MCU is affective) and you can read the pin status back (if external device has tied low)

Break it down, how generate and sample such a waveform.

If the sensor sends you a 0 or a 1 is given by the duration how long (in time) the pin is 0 or 1.

Now, you could sample with the fastest speed, e.g. every X micro-sec. for the shortest period (e.g. a low bit). You sample with a constant speed and you get a bit stream (store it in memory):
now you can post-process the bits in memory: if you see a 101010 - it might be a sequence of bits as 0 from sensor, if it is 111111 it was a sequence of bits as 1 from sensor. If you see 10111011 - it was a sequence of bits like 0 1 0 1. Just analyze the duration and bit pattern in memory to "decode" the reponse.

You could also use GPIO interrupts plus a timer (TIM): set (or toggle) GPIO pin for falling and/or raising edge on signal and measure the time between the GPIO INTs: was it a long period - a 1 bit received, was it a short period - a 0 bit received.

Just check out what "Single Wire Interface" (SWI) is, if your MCU has support for it, or try to emulate via GPIO by "sampling" a bit sequence and do a post-processing.

BTW: you cannot really debug with steps or pausing the FW running: you can debug only on the final result. But stopping the SW (except, you would have a real SWI in MCU) will result in lost bits.

But if you use INTs, e.g. with falling and raising edge: you store also "time stamps" in memory. Later. you can use the "time stamps" in order to "measure" the duration, in order to realize a 0 vs. 1 sent from sensor.

A debugger cannot stop the sensor sending bit streams: you have to let it come in and verify later if you see the right bit pattern.

Andrew Neil
Super User
Feb 23, 2024 5:46 PM UTC

@tjaekel wrote:

A debugger cannot stop the sensor sending bit streams: you have to let it come in and verify later if you see the right bit pattern.


Maybe; maybe not (entirely):

As the microcontroller is the Master, it "pulls" the data from the sensor - rather than the sensor just "pushing" it out.

I don't know the details of this interface but, with the Dallas 1-Wire(TM), it was only the timing within each bit that was critical - so you could halt the Master between bits...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Feb 23, 2024 5:42 PM UTC

@pablo1409 wrote:

I don't know how to debug this. I don't know how to see if I my sensor is sending me data. 


You'll need an oscilloscope or logic analyser to see what the sensor's actually doing

As @tjaekel suggests, it's a widely-used sensor, so there's plenty of references and examples to look at ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.