Skip to main content
Associate III
March 14, 2024
Solved

How to read ADC without DMA ?????

Board: NUcleo 64-G474

 

 

I just want to read 2 channels of an ADC but am presented with a bewildering array of incredibly confusing options: Ranks, Continuous mode, discontinous mode, number of conversions, oversampling, triggers, etc, etc, etc. The embedded "help" is completely useless.

I have two SE channels of ADC1 enabled (1 and 2), and I want to sample them both NOT in DMA. Seems reaonsonable but after hours of trying I can find nothing that works, and no resources to help. I'm trying the code below and various offshoots of it.

 

  while (1)
  {
 
  HAL_ADC_Start(&hadc1); // start the adc
  HAL_ADC_PollForConversion(&hadc1, 1000); // poll for conversion
  adc1_val = HAL_ADC_GetValue(&hadc1); // get the adc value
 
  HAL_ADC_Start(&hadc1); // start the adc
  HAL_ADC_PollForConversion(&hadc1, 1000); // poll for conversion
  adc2_val = HAL_ADC_GetValue(&hadc1); // get the adc value
  HAL_ADC_Stop(&hadc1); // stop adc
 
   printf("adc=[%d, %d]\n\r", adc1_val, adc2_val);

 

 

 

sgordon777_0-1710460374786.png

 

This topic has been closed for replies.
RomainR.
RomainR.Best answer
ST Employee
March 15, 2024

Hi @sgordon777 

Here in attached my example to use ADC1 Channel1 & Channel2 without DMA (PA0 & PA1)

You can test it on your side (STM32CubeIDE and Nucleo-G474RE)

If you need to build the project, ask OK to build without invoking Device Configuration Tool code generation by CubeMX.

RomainR_0-1710518007346.png

The reason is because the initial Mx configuration has been overwritten in the code.

I hope it will help you?

Thank you to give your feedback.
Best regards,

Romain

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

RomainR.
RomainR.Best answer
ST Employee
March 15, 2024

Hi @sgordon777 

Here in attached my example to use ADC1 Channel1 & Channel2 without DMA (PA0 & PA1)

You can test it on your side (STM32CubeIDE and Nucleo-G474RE)

If you need to build the project, ask OK to build without invoking Device Configuration Tool code generation by CubeMX.

RomainR_0-1710518007346.png

The reason is because the initial Mx configuration has been overwritten in the code.

I hope it will help you?

Thank you to give your feedback.
Best regards,

Romain

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
March 15, 2024

Thanks

 

RomainR.
ST Employee
March 16, 2024

Hi @sgordon777 

Does this help you? Any feedback?

BR

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.