Skip to main content
almog.itzko
Associate II
October 21, 2018
Question

How to properly use SPI communication in STM32L053 ??

  • October 21, 2018
  • 5 replies
  • 1229 views

Hello.

I am working on a project and using STM32L053 board.

For now, my goal is to create a channel of SPI communication, master & slave, an to test my code.

I am using only 1 ST board which serves both as master and slave. 

I have defined all necessary GPIOs using the CubeMX program - miso, mosi, clk, (software nss).

As part of the requirements i need to use the DMA in order to transmitte and receive date.

Each SPI has it's own Rx & Tx buffers which are connected to the relevant channel of the DMA.

The problem:

I have been able to send data only in one direction: Master --> Slave - I load the Tx buffer of the master and send it to the slave. The slave receives it properly into it's Rx buffer. I also see the DMA channels do what they are suppose to do.

The other way around does not seem to work. No matter what i have tried, the master wont get back a reply for the slave.

Any ideas to what should i pay more attention or check in my code ??

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    October 21, 2018

    The master has to shift data out, or otherwise generate a clock, for the slave to be able to respond.

    This is often achieved by sending dummy data.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    almog.itzko
    Associate II
    October 21, 2018

    Thank you for your answer.

    Of course i have tried doing that. My current test is sending a few messages one after the other, one is valid and the other is a dummy.

    The data does not shift back to the master in this case.

    At first i thought that my DMA initialization was wrong but i went over my parameters many times and they are ok.

    waclawek.jan
    Super User
    October 21, 2018

    Do you see the data coming from slave on the MISO line when observed by an oscilloscope/logic analyzer?

    Do you see those data in the data register of SPI in a debugger? (But don't look at SPI registers by debugger when you want the DMA to work).

    JW

    almog.itzko
    Associate II
    October 22, 2018

    No, i cant see the MISO line when observed by an oscilloscope.

    When i send data from master to slave, at the end of the transmission i can see inside the slave's DR the last char that was sent.

    almog.itzko
    Associate II
    October 22, 2018

    I think i found the problem.

    I seems that the master's Rx and slave's Tx should always be enabled during the entire process.

    Previously i have enabled them in different places in my code, now i enabling the relevant DMA channels in the beginning, where i initialize all DMA parameters and never touch them again.

    Thank you