Skip to main content
EWarzocha
Visitor II
October 25, 2022
Question

How to properly configure ADC injected group?

  • October 25, 2022
  • 0 replies
  • 591 views

Hello, I've tried to use ADC for two Potentiometers only with injected group conversion but couldn't make it work. I'm using STM32F446RE. I couldn't find solution so I'm asking here.

Previously I read their value correctly via polling and I know that rest of my code is working (there is not much else there, all the code related to ADC is below).

Am I missing something or the order of code is incorrect? The print in interrupt prints zeroes so the interrupt itself runs.

I'm using prescaler because APB2 clock is set to 90 Mhz and prescaler solved issues with reading interference.

Thanks in advance.

#define PA0_ADC_MODE (3 << 0)
#define PA1_ADC_MODE (3 << 2)
#define ADC1EN (1 << 8)
#define ADON (1 << 0)
 
#define ADC_CLOCK_PRESCALER_8 (3 << 16)
 
#define SWSTART (1 << 30)
#define JSWSTART (1 << 22)
#define EOCIE (1 << 5)
#define JEOCIE (1 << 7)
 
#define SCAN_MODE (1 << 8)
#define JAUTO (1 << 10)
#define CONTINUOUS_MODE (1 << 1)
 
#define INJECTED_GROUP_NUMBER_OF_CHANNELS_2 (1 << 20)
#define QUEUE3_CH0 ( 0 << 10)
#define QUEUE4_CH1 (1 << 15)
 
void adc_init_injected_group(){
 RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN_Msk;
 RCC->APB2ENR |= ADC1EN;
 
 GPIOA->MODER |= PA0_ADC_MODE;
 GPIOA->MODER |= PA1_ADC_MODE;
 
 ADC->CCR |= ADC_CLOCK_PRESCALER_8;
 ADC1->CR2 |= ADON;
 
 ADC1->JSQR |= INJECTED_GROUP_NUMBER_OF_CHANNELS_2;
 ADC1->JSQR |= QUEUE3_CH0;
 ADC1->JSQR |= QUEUE4_CH1;
 
 ADC1->CR1 |= SCAN_MODE; 
 ADC1->CR1 |= JAUTO;
 ADC1->CR2 |= CONTINUOUS_MODE;
 
 ADC1->CR2 |= SWSTART;
 ADC1->CR2 |= JSWSTART;
 
 ADC1->CR1 |= EOCIE;
 ADC1->CR1 |= JEOCIE; 
 
 NVIC_EnableIRQ(ADC_IRQn);
}
 
void ADC_IRQHandler(void){
 if(ADC1->SR & ADC_SR_JEOC){
 ADC1->SR &=~ ADC_SR_JEOC;
 volatile uint32_t values[2];
 values[0] = ADC1->JDR3;
 values[1] = ADC1->JDR4;
 
 printf("Values: %d, %d\n\r", (int)values[0], (int)values[1]);
 
 }
}

This topic has been closed for replies.