Skip to main content
Sashvat
Associate III
May 2, 2019
Question

How to program an STM32 ARM micro controller

  • May 2, 2019
  • 15 replies
  • 4250 views

Hi guys, I have a project where I need to use STM32 ARM processors I want to be able to program a bare chip of STM32's ARM Microcontrollers on my breadboard. I have a ST link V2 as the programmer. I would like to know what software (for free only)/application I need to install on my computer to code and upload it to this bare chip of mine. What are the steps I need to take to successfully write code and dump it on my STM32 ARM Microcontroller.

To basically sum it up, I have a LCD display, and I want to display characters from a sensor's readings, so which software do I use to write and upload code and it should be used with my ST link v2.

Thank you.

    This topic has been closed for replies.

    15 replies

    LACTIC
    Associate III
    May 2, 2019

    If you want to work with HAL library then use STM32CUBEMX which is free of cost, this help you to make skeleton of program . You can also use Standard Peripheral library which is easy but take time to understand. IDE you can use KEIL, ATOLIC, SYTEMWORK BENCH and CoCox. its depend on you.

    Sashvat
    SashvatAuthor
    Associate III
    May 3, 2019

    Does a bare STM32 ARM chip come with a boot loader installed? or do I need to program one for it to work? Whats the procedure to do it?

    LACTIC
    Associate III
    May 2, 2019

    Which type of LCD is that means 16x2 or graphical type.

    Sashvat
    SashvatAuthor
    Associate III
    May 2, 2019

    its a 16x2 LCD display

    Sashvat
    SashvatAuthor
    Associate III
    May 2, 2019

    Where can I download Keil from? what is the exact software I need to use?

    LACTIC
    Associate III
    May 3, 2019

    Below is arm keil link download from here:-

    https://www2.keil.com/stmicroelectronics-stm32/mdk

    For interfacing of 16x2 LCD you got support from youtube or by github.

    Sashvat
    SashvatAuthor
    Associate III
    May 3, 2019

    Can I follow the same code as what this video shows? (look at 5:27 for what I am talking about) https://www.youtube.com/watch?v=877SPdwuuLA&list=PL6PplMTH29SHgRPDufZhfMRoFwRAIrzOp&index=27

    And does a bare chip from STM come with the boot loader installed or do I have to make my own boot loader program?

    MikeDB
    Senior II
    May 7, 2019

    What is the STM32 model ? From what you describe it's a simple application so if it's a supported model Arduino might be a far easier to use IDE/programmer than STMCube.

    Sashvat
    SashvatAuthor
    Associate III
    May 8, 2019

    I am looking at seeing all cortex ARM processors from M0 to M7 and program them to find which is best suited.