Skip to main content
cyril2399
Associate III
Jul 12, 2011 7:24 AM UTC
Question

how to program a potentiometer

Posted on July 12, 2011 at 09:24

hello,

I have the STM3210C eval board and there is a potentiometer linked at PC4.

I want to divide all the range into ten parts.

What should I do ?

I have try to do Read Input Data, and all the function ''read...'' present in stm32f10x_gpio.c

PC4 is always at zero....

Thank to all
    This topic has been closed for replies.

    5 replies

    Andrew Neil
    Super User
    Jul 12, 2011 8:26 AM UTC
    Posted on July 12, 2011 at 10:26

    A potentiometer will give you an analogue signal; GPIOs are digital  !

    Look at the examples included with the Standard Peripheral Library...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    cyril2399
    cyril2399Author
    Associate III
    Jul 12, 2011 8:50 AM UTC
    Posted on July 12, 2011 at 10:50

    which example should I look?

    thanks

    Andrew Neil
    Super User
    Jul 12, 2011 10:29 AM UTC
    Posted on July 12, 2011 at 12:29

    I suggest that you invest some time in taking a look through all  of them - to familiarise yourself with what's available.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    raptorhal2
    Lead
    Jul 12, 2011 1:34 PM UTC
    Posted on July 12, 2011 at 15:34

    When you get stuck on something, always Read The Fine Manual first.

    And after you follow Andrew's advice, go to the STM32F105/7 data sheet, Section 3 Pin Descriptions, Table 5 Pin Definitions where you will see that PC4 in alternate function mode is ADC channel 14.

    Then go to RM0008 Reference Manual Section 9 that describes alternate functions.

    This documentation is available on ST's web site associated with the processor you are using.

    Cheers, Hal

    raptorhal2
    Lead
    Jul 12, 2011 1:34 PM UTC
    Posted on July 12, 2011 at 15:34

    When you get stuck on something, always Read The Fine Manual first.

    And after you follow Andrew's advice, go to the STM32F105/7 data sheet, Section 3 Pin Descriptions, Table 5 Pin Definitions where you will see that PC4 in alternate function mode is ADC channel 14.

    Then go to RM0008 Reference Manual Section 9 that describes alternate functions.

    This documentation is available on ST's web site associated with the processor you are using.

    Cheers, Hal