Skip to main content
MetuPhysics
Associate II
October 21, 2022
Question

How to print "Hello ARM World!" by using (C++) gcc compiler in STM32F4 discovery board?

  • October 21, 2022
  • 1 reply
  • 640 views

For example:

#include <iostream>

using namespace std;

int

main()

{

 cout << "Hello Arm World!" << endl;

 return 0;

}

Can u give detailed info step by step?..

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
October 21, 2022

>>Can u give detailed info step by step?

Sorry I'm more Fight Club than Kindergarten Cop..

You have to initialize the hardware and do the plumbing.

So clocks, pins, peripherals, for the UART you plan to use. The STM32F407-DISCO doesn't have a built in VCP with the ST-LINK/V2. You could perhaps use the SWV (SWO PB3) route, but you'd need to check the wiring/solder-bridge situation. I used the break-out board STM32F4DIS-BB, it had a RS232 DB9 via USART6

Have a newlib.c supporting _read() / _write(), in ST's typical approach these should call __io_putchar() and __io_getchar(), based on GNU's implementation of STDIO

Here an SPL implementation (circa 2017)

/** @addtogroup STM32401_DISCOVERY_LOW_LEVEL_COM
 * @{
 */
#define COMn 1
 
/**
 * @brief Definition for COM port1, connected to USART6 (STM32F4DIS-BB)
 */
#define EVAL_COM1 USART6
#define EVAL_COM1_CLK RCC_APB2Periph_USART6
#define EVAL_COM1_TX_PIN GPIO_Pin_6
#define EVAL_COM1_TX_GPIO_PORT GPIOC
#define EVAL_COM1_TX_GPIO_CLK RCC_AHB1Periph_GPIOC
#define EVAL_COM1_TX_SOURCE GPIO_PinSource6
#define EVAL_COM1_TX_AF GPIO_AF_USART6
#define EVAL_COM1_RX_PIN GPIO_Pin_7
#define EVAL_COM1_RX_GPIO_PORT GPIOC
#define EVAL_COM1_RX_GPIO_CLK RCC_AHB1Periph_GPIOC
#define EVAL_COM1_RX_SOURCE GPIO_PinSource7
#define EVAL_COM1_RX_AF GPIO_AF_USART6
#define EVAL_COM1_IRQn USART6_IRQn
 
...
 
USART_TypeDef* COM_USART[COMn] = {EVAL_COM1};
 
GPIO_TypeDef* COM_TX_PORT[COMn] = {EVAL_COM1_TX_GPIO_PORT};
 
GPIO_TypeDef* COM_RX_PORT[COMn] = {EVAL_COM1_RX_GPIO_PORT};
 
const uint32_t COM_USART_CLK[COMn] = {EVAL_COM1_CLK};
 
const uint32_t COM_TX_PORT_CLK[COMn] = {EVAL_COM1_TX_GPIO_CLK};
 
const uint32_t COM_RX_PORT_CLK[COMn] = {EVAL_COM1_RX_GPIO_CLK};
 
const uint16_t COM_TX_PIN[COMn] = {EVAL_COM1_TX_PIN};
 
const uint16_t COM_RX_PIN[COMn] = {EVAL_COM1_RX_PIN};
 
const uint16_t COM_TX_PIN_SOURCE[COMn] = {EVAL_COM1_TX_SOURCE};
 
const uint16_t COM_RX_PIN_SOURCE[COMn] = {EVAL_COM1_RX_SOURCE};
 
const uint16_t COM_TX_AF[COMn] = {EVAL_COM1_TX_AF};
 
const uint16_t COM_RX_AF[COMn] = {EVAL_COM1_RX_AF};
 
...
 
/**
 * @brief Configures COM port.
 * @param COM: Specifies the COM port to be configured.
 * This parameter can be one of following parameters:
 * @arg COM1
 * @arg COM2
 * @param USART_InitStruct: pointer to a USART_InitTypeDef structure that
 * contains the configuration information for the specified USART peripheral.
 * @retval None
 */
void STM_EVAL_COMInit(COM_TypeDef COM, USART_InitTypeDef* USART_InitStruct)
{
 GPIO_InitTypeDef GPIO_InitStructure;
 
 /* Enable GPIO clock */
 RCC_AHB1PeriphClockCmd(COM_TX_PORT_CLK[COM] | COM_RX_PORT_CLK[COM], ENABLE);
 
 if ((COM_USART[COM] == USART1) || (COM_USART[COM] == USART6))	/* APB2 USARTs */
 {
 /* Enable UART clock on APB2 */
 RCC_APB2PeriphClockCmd(COM_USART_CLK[COM], ENABLE);
 }
	else
 {
 /* Enable UART clock on APB1 */
 RCC_APB1PeriphClockCmd(COM_USART_CLK[COM], ENABLE);
 }
 
 /* Connect PXx to USARTx_Tx*/
 GPIO_PinAFConfig(COM_TX_PORT[COM], COM_TX_PIN_SOURCE[COM], COM_TX_AF[COM]);
 
 /* Connect PXx to USARTx_Rx*/
 GPIO_PinAFConfig(COM_RX_PORT[COM], COM_RX_PIN_SOURCE[COM], COM_RX_AF[COM]);
 
 /* Configure USART Tx as alternate function */
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 
 GPIO_InitStructure.GPIO_Pin = COM_TX_PIN[COM];
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
 GPIO_Init(COM_TX_PORT[COM], &GPIO_InitStructure);
 
 /* Configure USART Rx as alternate function */
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 GPIO_InitStructure.GPIO_Pin = COM_RX_PIN[COM];
 GPIO_Init(COM_RX_PORT[COM], &GPIO_InitStructure);
 
 /* USART configuration */
 USART_Init(COM_USART[COM], USART_InitStruct);
 
 /* Enable USART */
 USART_Cmd(COM_USART[COM], ENABLE);
}
 
...
 
//******************************************************************************
 
void USART_Configuration(void)
{
	USART_InitTypeDef USART_InitStructure;
 
 /* USARTx configured as follow:
 - BaudRate = 115200 baud
 - Word Length = 8 Bits
 - One Stop Bit
 - No parity
 - Hardware flow control disabled (RTS and CTS signals)
 - Receive and transmit enabled
 */
 USART_InitStructure.USART_BaudRate = 115200;
 USART_InitStructure.USART_WordLength = USART_WordLength_8b;
 USART_InitStructure.USART_StopBits = USART_StopBits_1;
 USART_InitStructure.USART_Parity = USART_Parity_No;
 USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
 USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
 
 STM_EVAL_COMInit(COM1, &USART_InitStructure);
}
 
//******************************************************************************
 
/**
 * @brief Retargets the C library printf function to the USART (GNU)
 * @param None
 * @retval None
 */
int __io_putchar(int ch)
{
 /* Place your implementation of fputc here */
 /* e.g. write a character to the USART */
 
	ITM_SendChar(ch); // SWV
 
 /* Loop until the transmit buffer empty */
 while (USART_GetFlagStatus(EVAL_COM1, USART_FLAG_TXE) == RESET)
 {}
 
 USART_SendData(EVAL_COM1, (uint8_t) ch);
 
 return(ch);
}
 
//******************************************************************************
 
/**
 * @brief Retargets the C library scanf function to the USART (GNU)
 * @param None
 * @retval None
 */
int __io_getchar(void)
{
 /* Place your implementation of fgetc here */
 /* e.g. read a character from the USART */
 
 /* Loop until the receive buffer not empty */
 while (USART_GetFlagStatus(EVAL_COM1, USART_FLAG_RXNE) == RESET)
 {}
 
 return((int)USART_ReceiveData(EVAL_COM1));
}
 
//******************************************************************************

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..