Skip to main content
C S
Associate II
October 25, 2017
Question

How to operate DAC at update speed of 1MSPS?

  • October 25, 2017
  • 8 replies
  • 2580 views
Posted on October 25, 2017 at 06:56

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    8 replies

    AvaTar
    Senior III
    October 25, 2017
    Posted on October 25, 2017 at 07:53

    When I set update rate to 500ksps, I get triangular wave which has uneven slope. Can anyone tell me what should I do to resolve this and what should I do to get my code running as desired?

    Reduce output rate. You ignored the settling time of the DAC, i.e. it's bandwidth.

    The F405/407 for example specifies 3 .. 6us.

    C S
    C SAuthor
    Associate II
    October 25, 2017
    Posted on October 25, 2017 at 08:19

    By output rate, do you mean update rate of DAC? Actually I need DAC running at 1MSPS. Reducing speed of DAC is not an option unfortunately. 

    Besides, it is mentioned that DAC speed can be as kept as high as 1 MSPS for my board.

    S.Ma
    Principal
    October 25, 2017
    Posted on October 25, 2017 at 08:01

    Check for the DAC maximum slew rate, activate the output buffer and remember to check the output signal without loading the output too much (a follower op-amp would simplify things before optimizing).

    On my side, I usually use a Timer output compare pin and feed it through the DAC trigger input pin. This way, I can manually play with a jumper wire and debug the DAC manually. If later using ADC, they too uses a different input trigger pin, so it is possible to tune ADC/DAC sampling skew.

    C S
    C SAuthor
    Associate II
    October 25, 2017
    Posted on October 25, 2017 at 08:21

    I already have output buffer activated. So it should not be a problem,right?

    AvaTar
    Senior III
    October 25, 2017
    Posted on October 25, 2017 at 08:41

    So it should not be a problem,right?

    It is.

    Surely you can stuff words faster into the DR register, but the actual DA converter electronics is the slowest element in this chain.

    The L476 has a typical settling time of 2us - check the datasheet.

    You cannot beat Nyquist.