How to map STM32G0B0 DMA to UART1 TX
- STM32CubeIDE Version: 1.12.0
- Using LL drivers
- ADC to Memory via DMA1 Channel1 working
- USART1 RX works
- Memory to USART1 TX via DMA1 Channel2 does not work
I'm guessing the problem we are having is that we are not using the correct DMA channel for USART1 TX but RM0454, STM32G0B0KE/CE/RE/VE data sheet and PM0223 do not have a table for the mapping. It probably has something to do with the DMAMUX which we have not seen before, but how can these documents cover DMA operation and not reference the correct mappings? It is possible that there is some type of ordering that is incorrect but we have found no examples that use USART's with DMA's. If someone could clue us in as to what we are missing it would be greatly appreciated.
LL_USART_InitTypeDef USART_InitStruct = {0};
// USART configuration
// BaudRate = 115200 baud, Word Length = 8 Bits
// One Stop Bit, No parity,
// Hardware flow control disabled (RTS and CTS signals)
//Receive and transmit enabled
USART_InitStruct.PrescalerValue = LL_USART_PRESCALER_DIV1;
USART_InitStruct.BaudRate = 38400;
USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
USART_InitStruct.Parity = LL_USART_PARITY_NONE;
USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_SetTXFIFOThreshold(USART1, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_SetRXFIFOThreshold(USART1, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_DisableFIFO(USART1);
LL_USART_ConfigAsyncMode(USART1);
/* Enable USART */
LL_USART_Enable(USART1);
/* Enable the USART1 Tx DMA1 requests */
//USART_DMACmd(USART1, USART_DMAReq_Tx, ENABLE);
// USe DMA to transmit the serial data
// DMA configuration for TX of serial tx buffer(Serial TX, outbound)
// Configure DMA request MEMTOMEM_DMA1_Channel2
// Set request number, Set transfer direction, Set priority level, Set DMA mode, Set peripheral increment mode,
// Set memory increment mode, Set peripheral data width, Set memory data width
LL_DMA_SetPeriphRequest(DMA1, LL_DMA_CHANNEL_2, LL_DMAMUX_REQ_USART1_TX);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_2, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PRIORITY_HIGH);
LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MODE_NORMAL);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PDATAALIGN_BYTE);
LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PDATAALIGN_BYTE);
LL_DMAMUX_SetRequestID(DMAMUX1, LL_DMAMUX_CHANNEL_2, LL_DMAMUX_REQ_USART2_TX);
LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_2, (uint32_t)txBuffer,
LL_USART_DMA_GetRegAddr(USART1, LL_USART_DMA_REG_DATA_TRANSMIT),
LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
// Enable transfer complete and transfer error interrupts.
LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_2);
LL_DMA_EnableIT_TE(DMA1, LL_DMA_CHANNEL_2);
/* DMA1 Channel2 enable */
LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_2);