Skip to main content
JGale
Associate
Jul 24, 2019 8:52 AM UTC
Question

How to make partition binaries for STM32F103ZC using Makefiles

I just switched from Arduino to the ST HAL library, I'm quite new to both the structure and makefiles in general. I'm using a chip that allows for multiple parts that can be used for OTA's for example. While I have made a working project that can upload and run, I would also like to build separate binaries for the different parts (Bootloader, Part0, Part1). With Arduino I could just select the part and build a binary that way. I can't find a way to get these building commands to work with the new library, does someone know anything on how to make this work.

Update:

The partitions are probably indicated by the linkerScript. I've made three different ones (Flash, Part0 and Part1) these have different configurations when it comes to size and flash location.

I now want to compile the whole project using these linkerScripts without having to change the linker scripts name everytime, so that is where I'm kinda stuck now.

This topic has been closed for replies.