Question
How to make a master PWM that vary duty cycle from 1 to 35% and have phase shift with two other pwm?
We need to make a master PWM that vary duty cycle from 1 to 35% and have a phase shift with two other pwm (this two other pwm are in phase and duty cycle 50%, but one starts with one and other starts wiht zero.). The phase shift should vary from 1 to 360 degrees. All the pwm have the same frequency and should be possible change the frequency for all. I tryed output compare between 3 pwm, but only works at 50% duty cycle.