Skip to main content
Associate
Dec 23, 2024 4:57 AM UTC
Solved

How to load the external QSPI using USB-DFU method

Hello

Controller - STM32H745

We are using an external QSPI to store the application image. Currently we are flashing the image using JTAG and .stldr file as an argument to cmd ln utility STM32_Programmer_CLI.exe 

When I pull the boot0 pin HIGH I am able to load the internal flash. Is there a possibility to flash the external QSPI using USB-DFU method?

I tried this cmd but it didn't work and help section of the STM32_Programmer_CLI.exe is not clear about this topic

STM32_Programmer_CLI.exe -c port=USB1 pid=0xDF11 vid=0x0483 -w "%FW_FILE_PATH%App-CM7.hex" -v -el "%FW_FILE_PATH%qspiflashLoader-CM7.stldr"

 

This topic has been closed for replies.
Ethan HUANG
Ethan HUANGBest answer
ST Employee
Dec 23, 2024 5:32 AM UTC

According to the NOTE in Section 3.2.13 (External loader command) in UM2237 (Rev 24), using external loader over bootloader interface is not supported:

NOTE: This command (-el) is only supported with SWD/JTAG ports.

11 replies

Ethan HUANG
Ethan HUANGBest answer
ST Employee
Dec 23, 2024 5:32 AM UTC

According to the NOTE in Section 3.2.13 (External loader command) in UM2237 (Rev 24), using external loader over bootloader interface is not supported:

NOTE: This command (-el) is only supported with SWD/JTAG ports.

Tesla DeLorean
Guru
Dec 23, 2024 5:01 PM UTC

Isn't the path here to create your own USB DFU Device implementation supporting/reporting the memory regions in your design?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Madhav_1Author
Associate
Dec 24, 2024 6:24 AM UTC

No, first I wanted to understand if there is a possibility of using internal ROM Bootloader to load the external QSPI flash using the USB.

Ethan's answer clarifies that its not possible.

Can you suggest any example projects to achieve your own USB DFU Device implementation supporting/reporting the memory regions in your design?

MM..1
Super User
Dec 24, 2024 7:30 AM UTC

Technicaly one simple way exist , based on how big image you require load. Idea is place image into imNx.hex with flasher code. Load over DFU and run. Wait for flashing to ext and load next hex as internal or next part ext...

For big external image load some intermediate fw ... that open some protocol and load ext. Then DFU internal back.

For some size you can DFU to ram and run, require more finness