Skip to main content
Jack Li
Associate
Jun 28, 2017 1:19 AM UTC
Solved

HOW to let CAN1 using all 28 filter banks?

Posted on June 28, 2017 at 03:19

Dear all

Useing CAN1 of STM32F205, 32-bit Mask Mode filter, filter bank 0-13 work all right for now.

Then I am trying to configurate CAN2SB = 28d, for letting CAN1 use all 28 filter banks.

But it doesn't work, here is my part of code, would you please help me?

Thx inadvance

void    can_Init(void)

{

UCHAR i;

    RCC->APB1ENR  |= RCC_APB1ENR_CAN1EN;                                // Enable clock for CAN

    RCC->APB1RSTR |= RCC_APB1RSTR_CAN1RST;                              // Reset CAN module

    

    RCC->APB1RSTR &= ~RCC_APB1RSTR_CAN1RST;                             // Deactivate reset

    CAN1->MCR = CAN_MCR_ABOM | CAN_MCR_INRQ;                            // Automatic bus-off managment, init request

    CAN1->IER = CAN_IER_FMPIE0 | CAN_IER_FMPIE1;                        // Active interrupts

                                                    

    CAN1->BTR = ( ((CAN_1tq) << 24)    | ((CAN_4tq) << 20)

                | ((CAN_3tq) << 16)  | (((APB1_CLK/(CAN_TQS * CAN_BITRATE)) -1) & 0x3ff) );       // Set bit timing

    CAN1->FMR  |= CAN_FMR_FINIT;                                        // Set filter init, do default filter setup

    CAN1->FMR &= ~CAN_FMR_CAN2SB;

    CAN1->FMR  |= (CAN_FMR_CAN2SB & (0x1C << 8));                                       // all the filters to CAN1 can be used.

    CAN1->FM1R  = 0x00000000;                                           // Set all filters in Identifier mask mode

    CAN1->FS1R  = 0x0fffffff;                                           // Set all filters to 32 bit

    CAN1->FFA1R = 0x0aaaaaaa;                                           // Even filters to FIFO0, odd filters to FIFO1

    CAN1->FA1R  = 0x00000000;                                           // Disable all receive filters

    CAN1->FMR  &= ~ CAN_FMR_FINIT;                                      // Clear filter init

    NVIC_SetPriority(CAN1_RX0_IRQn,CAN_PRIO);

    NVIC_EnableIRQ(CAN1_RX0_IRQn);                                      // Enable FIFO 0 interrupt

    NVIC_SetPriority(CAN1_RX1_IRQn,CAN_PRIO);

    NVIC_EnableIRQ(CAN1_RX1_IRQn);                                      // Enable FIFO 1 interrupt

    CAN1->MCR &= ~ CAN_MCR_INRQ;                                        // End of initialization

    GPIOB->BSRR = GPIO_BSRR_BR_6;                                               // CAN_S low

    for(i = 0;i < CAN_NROF_RXMSG;i++){

        can_buf_wptr[i] = 0;

        can_buf_rptr[i] = 0;

    }

}

// Setup and enable receive filter with index msg_index

void    can_SetupFilter(UCHAR msg_index, UCHAR idsize, ULONG canid, ULONG mask)

{

ULONG              id_val, mask_val;

volatile ULONG *   can_filter_ptr;

UCHAR               filter_index;

    if (msg_index < CAN_NROF_FILTERS){

        can_filter_ptr = &CAN1->sFilterRegister[0].FR1;                // Pointer to first register in filter bank

        filter_index = msg_index * 2;

        if (idsize == CAN_STD_ID){

            id_val   = (canid << 21);  

            mask_val = (mask  << 21);

        } else {

            id_val   = (canid << 3) | 0x04;         // Id with IDE bit set  

            mask_val = (mask << 3)  | 0x04;

        }

        CAN1->FA1R &= ~ (1 << msg_index);             // Deactivate filter

        can_filter_ptr[filter_index] = id_val;      // Set id

        can_filter_ptr[filter_index+1] = mask_val;  // Set mask

        CAN1->FA1R |= (1 << msg_index);               // Activate filter

    }

}
    This topic has been closed for replies.
    Jack Li
    Jack LiBest answer
    Associate
    Jun 29, 2017 1:38 AM UTC
    Posted on June 29, 2017 at 03:38

    after investigated

    a litlle further by studying the code ST uses in their standard peripheral library. It seems CAN2SB has to be in the range 1-27 not 28 as the RM says. When I set CAN2SB as 0x1B, it allows CAN1 using NO.0-26 filter banks.

    1 reply

    Jack Li
    Jack LiAuthorBest answer
    Associate
    Jun 29, 2017 1:38 AM UTC
    Posted on June 29, 2017 at 03:38

    after investigated

    a litlle further by studying the code ST uses in their standard peripheral library. It seems CAN2SB has to be in the range 1-27 not 28 as the RM says. When I set CAN2SB as 0x1B, it allows CAN1 using NO.0-26 filter banks.