Skip to main content
Associate II
October 5, 2024
Question

How to Interface IMP34DT05TR Mic with STM32G473VET6 and Save Audio as .WAV

Hello,

I am working with STM's IMP34DT05TR microphone in stereo configuration using the STM32G473VET6 microcontroller. I would like to record audio and save it in a .wav file format.

Could anyone provide guidance on how to interface the microphone with the microcontroller and the best approach to record the audio and store it as a .wav file?

Any code samples or pointers to relevant documentation would be greatly appreciated!

Thanks in advance!

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
October 8, 2024

Hello @AiROT and welcome to the Community,

 

I recommend you to take a look at these examples in STM32CubeF4 Firmware and get inspired to configure your own project.

  • \STM32Cube_FW_F4_V1.28.1\Projects\STM32F411E-Discovery\Examples\BSP
  • \STM32Cube_FW_F4_V1.28.1\Projects\STM32F411E-Discovery\Applications\Audio\Audio_playback_and_record

These examples can help you to use ST MEMS microphone IMP34DT05TR  to record your voice.

Note that these applications have been tested with STMicroelectronics STM32F411E-Discovery board and can be easily tailored to any other supported device and development board.

 

I hope this help you.

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.