Skip to main content
MWide.1
Associate
Oct 15, 2020 6:12 PM UTC
Solved

How to install STM32Cube suite

The suite seems to consist of STM32CubeMX, STM32CubeIDE, STM32CubeProgrammer, STM32CubeMonitor, STM32Cube MCU Packages, and STM32Cube Expansion Packages. Do I need to download and install each of these separately, or is there a single installer that puts this whole "suite" or "ecosystem" on my PC at once? Also, if they are to be installed separately, does it matter in what order they are installed?

    This topic has been closed for replies.
    TDK
    TDKBest answer
    Oct 15, 2020 7:06 PM UTC

    Install CubeIDE which will install CubeMX. Within CubeIDE, you can install the MCU packages under the Help menu.

    CubeMX can also be installed separately and ran in standalone mode.

    CubeProgrammer is separate, although a version might be installed along with CubeIDE, not sure.

    CubeMonitor is separate.

    "If you feel a post has answered your question, please click ""Accept as Solution""."

    2 replies

    TDK
    TDKBest answer
    Oct 15, 2020 7:06 PM UTC

    Install CubeIDE which will install CubeMX. Within CubeIDE, you can install the MCU packages under the Help menu.

    CubeMX can also be installed separately and ran in standalone mode.

    CubeProgrammer is separate, although a version might be installed along with CubeIDE, not sure.

    CubeMonitor is separate.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    MWide.1
    MWide.1Author
    Associate
    Oct 15, 2020 7:19 PM UTC

    Thanks!