Question
How to increase SPI data size of STM32F107 to 24 bit ?
I'm working on STM32F107 microcontroller standard library and interfacing external ADC through SPI.
In SPI configuration , there are two data size, 8 bit and 16 bit as in below lines -
#define SPI_DataSize_16b ((uint16_t)0x0800)
#define SPI_DataSize_8b ((uint16_t)0x0000)
#define IS_SPI_DATASIZE(DATASIZE) (((DATASIZE) == SPI_DataSize_16b) || \
((DATASIZE) == SPI_DataSize_8b))
So how can I configure 24 data size?
please share the code