Skip to main content
juliuscaesar
Associate III
October 7, 2016
Question

How to import STM32Cube Firmware into a fresh openstm project

  • October 7, 2016
  • 1 reply
  • 629 views
Posted on October 07, 2016 at 13:56

Hey guys,

I downloaded the current Firmware (STM32Cube_FW_F4_V1.13.0) for my

32F429IDISCOVERY Board 

As a start i'd like to import a full demonstration. But when i try to import the SW4STM32 demonstration project the files are not copied to the workspace. Eclipse shows the code structure, but the are no files in my workspace (see pictures;))

The Checkbox copy projects into workspace is checked

http://share-your-photo.com/ced04b4e63

http://share-your-photo.com/dfff8b8d6d

So do you have any ideas how to get the missing files or is there a better way to start a new project (with HAL drivers, display driver and freeRTOS)?

greets Julian

    This topic has been closed for replies.

    1 reply

    slimen
    Visitor II
    October 7, 2016
    Posted on October 07, 2016 at 15:40

    Hello,

    You can start from working example under STM32CubeF4 firmware package, in the context of understanding the tools and you find the needed include parts for your project.

    STM32Cube_FW_F4_V1.13.0\Projects\STM32F429I-Discovery\Applications\FreeRTOS\FreeRTOS_ThreadCreation

    You can modify this working application depending on your needs.

    To open an existing project with SW4STM32 you should follow this steps below:

    • File >>Import

    • Existing Projects into workspace (>>Next)

    • Click on “Browse� for the root directory

    • The projects list is refreshed (select then your project)  

    • Ensure the option Copy projects into workspace is unchecked

    • Then click Finish.

    You can also use STM32CubeMX tool to initialize peripherals, build and generate your starting projects with initialization C code. This allow you to choose the microcontroller, select the peripherals that you want and map them to pins graphically. 

    For more detail about STM32CubeMX tool, review this user Manual

    http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM00104712.pdf/files/DM00104712.pdf/jcr:content/translations/en.DM00104712.pdf

     and this  section 4.12.6: FreeRTOS middleware configuration View section (page110).

    Regards