Skip to main content
AAgar.2
Associate III
Jun 10, 2020 8:12 PM UTC
Solved

How to handle HardFault?

There is a function called HardFault_Handler in the STM32 MCUs (full code below). This function I usually work with when debugging but am unsure how to use this for handling error. What is the correct protocol to handle errors in this function? If a fault has happened ideally I would like to clear the MCU ram and reset the MCU. However what if the handler code causes more faults. Is there a standard protocol for handling faults (not just HardFaults)?

void HardFault_Handler(void)
{
 /* USER CODE BEGIN HardFault_IRQn 0 */
 
 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_HardFault_IRQn 0 */
 /* USER CODE END W1_HardFault_IRQn 0 */
 }
}

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 10, 2020 8:19 PM UTC

You can technically return if you remediate the issue it faulted over, but that requires a very deep understanding of the CPU/ISA

What I normally do is output enough diagnostic information about registers, and perhaps a partial stack dump, so I can provide useful answers about the failure to the boss/customers rather than shrug my shoulders.

If you don't do anything complicated it shouldn't double-fault. Zeroing the imternal RAM using simple code (looping with internal registers, no function calls) should work fine.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jun 10, 2020 8:19 PM UTC

You can technically return if you remediate the issue it faulted over, but that requires a very deep understanding of the CPU/ISA

What I normally do is output enough diagnostic information about registers, and perhaps a partial stack dump, so I can provide useful answers about the failure to the boss/customers rather than shrug my shoulders.

If you don't do anything complicated it shouldn't double-fault. Zeroing the imternal RAM using simple code (looping with internal registers, no function calls) should work fine.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Jun 10, 2020 8:24 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..