Skip to main content
Associate II
April 17, 2024
Solved

How to get the value of the program counter ?

Hello,

 

Sometimes I have my stm32F7 going in hardfault_handler, so for my customers I have to display on a screen the last address where the software crashed, then I can analyse which problem occure the crash. So I want to get the value "pc" (program counter) like I can see in the Fault Analyzer of stm32cubeide.

 

I tried many supossed solutions :

__attribute__ ((__noinline__)) void *get_pc()
{
 return __builtin_return_address(0);
}

 or

static __inline__ void *get_pc(void)
{
 void *pc;
 asm("mov %0, pc" : "=r"(pc));
 return pc;
}

but it only return the value of the current function called, and not the same value as in the Fault Analyzer of stm32cubeide.

 

Is there a solution ?

 

Thank you

This topic has been closed for replies.
PierreG-SBest answer
Associate II
April 18, 2024

Ok for those who are intersted by a solution, I found what I wanted : get the program counter before the hardfault_handler, the same value as showed in the Fault Analyzer of stm32cubeide. I am worrking on a stm32f7 for information.

 

Here is the code in the function HardFault_Handler() :

// Put this struct in your ".h" 
typedef struct
{
 uint32_t r0;
 uint32_t r1;
 uint32_t r2;
 uint32_t r3;
 uint32_t r12;
 uint32_t lr;
 uint32_t pc;
 uint32_t psr;
} ExceptionStackFrame;

void HardFault_Handler(void)
{
 /* USER CODE BEGIN HardFault_IRQn 0 */

	uint32_t current_psp = __get_PSP();
	ExceptionStackFrame *hardfault_stack_frame = (ExceptionStackFrame *)(current_psp);
	uint32_t pc_value_at_fault = hardfault_stack_frame->pc;							 

 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_HardFault_IRQn 0 */
 /* USER CODE END W1_HardFault_IRQn 0 */
 }
}

2 replies

waclawek.jan
Super User
April 17, 2024

The PC value you are looking for is at the stack, so trick is to determine address of stack at fault handler entry, without C having disturbed that already.

@Tesla DeLorean  published this - note that despite Keil in its name there's a section telling how to do this using gcc, too.

JW

PierreG-SAuthorBest answer
Associate II
April 18, 2024

Ok for those who are intersted by a solution, I found what I wanted : get the program counter before the hardfault_handler, the same value as showed in the Fault Analyzer of stm32cubeide. I am worrking on a stm32f7 for information.

 

Here is the code in the function HardFault_Handler() :

// Put this struct in your ".h" 
typedef struct
{
 uint32_t r0;
 uint32_t r1;
 uint32_t r2;
 uint32_t r3;
 uint32_t r12;
 uint32_t lr;
 uint32_t pc;
 uint32_t psr;
} ExceptionStackFrame;

void HardFault_Handler(void)
{
 /* USER CODE BEGIN HardFault_IRQn 0 */

	uint32_t current_psp = __get_PSP();
	ExceptionStackFrame *hardfault_stack_frame = (ExceptionStackFrame *)(current_psp);
	uint32_t pc_value_at_fault = hardfault_stack_frame->pc;							 

 /* USER CODE END HardFault_IRQn 0 */
 while (1)
 {
 /* USER CODE BEGIN W1_HardFault_IRQn 0 */
 /* USER CODE END W1_HardFault_IRQn 0 */
 }
}