Skip to main content
Michael B
Associate III
Sep 26, 2019 11:59 PM UTC
Solved

How to get printf() float / double support working on F7

I've been fighting with this too long and can't figure it out. I've added uart communication for use with printf() by implementing the following in syscalls.c:

__attribute__((weak)) int _write(int file, char *ptr, int len)
{
 HAL_StatusTypeDef status = HAL_UART_Transmit(&huart1, (uint8_t *)ptr, len, 0xFFFF);
 return (status == HAL_OK ? len : 0);
}

That works fine with printf. But printing floats or doubles causes it to hang when it tries to output the number. I have enabled -u _printf_float in the MCU Settings of STM32CubeIDE (also tried adding it manually to the Linker flags).

double test = 1.2345;
printf("test: %f\r\n", test);
arm-none-eabi-g++ -o "ProjectTest.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"B:\gitrepo\ProjectTest\STM32F746NGHX_FLASH.ld" --specs=nosys.specs -Wl,-Map="ProjectTest.map" -Wl,--gc-sections -static -L../Middlewares/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -u _printf_float -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group

I don't really know how to debug this further, and I've read many relevant posts but nothing I've tried has worked. I really need it to, as the debugger in STM32CubeIDE is a pile of junk and the watcher shows incorrect values for variables.

Also note I'm using FreeRTOS here, not sure if it's an issue with stack alignment or how to debug that.

Help a brutha out?

This topic has been closed for replies.
Dave Nadler
Dave NadlerBest answer
Senior III
Sep 27, 2019 12:14 AM UTC

@Community member​ - Presuming you're using FreeRTOS or similar (you didn't say), the answer to your problem is most likely here:

https://community.st.com/s/question/0D50X0000BB1eL7SQJ/bug-cubemx-freertos-projects-corrupt-memory

http://www.nadler.com/embedded/newlibAndFreeRTOS.html

@Markus GIRDLAND​ - This is about one customer per week, no? And that's only the customers that ask on this forum.

Any updates as to when this will be fixed?

Also, I forgot to mention, please mention to your Architecture Team that NXP is shipping the heap_useNewlib I provided on my website with MCUxpresso.

@Community member​ - Please confirm this fixes your problem.

Hope this helps,

Best Regards, Dave

11 replies

Dave Nadler
Dave NadlerBest answer
Senior III
Sep 27, 2019 12:14 AM UTC

@Community member​ - Presuming you're using FreeRTOS or similar (you didn't say), the answer to your problem is most likely here:

https://community.st.com/s/question/0D50X0000BB1eL7SQJ/bug-cubemx-freertos-projects-corrupt-memory

http://www.nadler.com/embedded/newlibAndFreeRTOS.html

@Markus GIRDLAND​ - This is about one customer per week, no? And that's only the customers that ask on this forum.

Any updates as to when this will be fixed?

Also, I forgot to mention, please mention to your Architecture Team that NXP is shipping the heap_useNewlib I provided on my website with MCUxpresso.

@Community member​ - Please confirm this fixes your problem.

Hope this helps,

Best Regards, Dave

Michael B
Michael BAuthor
Associate III
Sep 27, 2019 12:16 AM UTC

That was fast, I was just adding the bit about FreeRTOS as you responded. I'll take a look at that and see if it helps out, will let you know!

Michael B
Michael BAuthor
Associate III
Sep 27, 2019 1:10 AM UTC

In a Stack Overflow style effort, I'll post a complete solution here (thanks to @Dave Nadler​ )!

As outlined in this link - it's a newlib problem with task concurrency in FreeRTOS that has yet to be patched, that was poorly implemented by ST, and is generated by CubeMX. Memory corruption occurs when using printf() and likely other things too, see the details on it at that link.

To fix:

  1. Exclude Src/sysmem.c
  2. Exclude Middlewares/Third_Party/Source/portable/MemMang/heap_4.c
  3. Add Src/heap_useNewLib.c (provided at the link above)

As a side note, I have added this to my STM32CubeIDE project patcher (1.0.2) too so you don't need to do this every time you generate code, at least until ST fixes their code.

AVI-crak
Senior
Sep 27, 2019 1:10 PM UTC

I ask you to check an alternative.

https://bitbucket.org/AVI-crak/sprint/src/default/sPrint.c

It should be noted that for simultaneous printing from multiple streams to one physical communication interface, it is necessary to win arbitration of access to this interface. At one point in time, only one thread should be able to use a physical port.

Pavel A.
Sep 29, 2019 8:05 PM UTC

Ah. Using C11 generics. Very cool =)

 But what is suffix 'd' on floating constants? No, it does not mean double. Is it a gcc extension? I googled but found only "decimal floating" which has suffixes like df or dd, but not a single d.

-- pa