Skip to main content
bruce
Associate III
September 13, 2008
Question

How to get into Standby Mode Simply

  • September 13, 2008
  • 2 replies
  • 746 views
Posted on September 13, 2008 at 19:53

How to get into Standby Mode Simply

    This topic has been closed for replies.

    2 replies

    bruce
    bruceAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:44

    I'm having trouble getting my stm32f101 into standby. Once there, I plan on waking up via a keypress on the wakeup pin, PA0.

    While the example code uses the RTC and EXTI, I would like to do something simpler.

    I tried:

    /* Enable PWR clock and wakeup pin */

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);

    PWR_WakeUpPinCmd(ENABLE);

    myprintf (''entering standby mode after 2 seconds\r\n'');

    PWR_EnterSTANDBYMode();

    When I run this, it appears to crash at this point, the oscillator stays running at full speed (HSI at 36mhz), I have a heartbeat LED driven off Timer1 IRQ and that keeps running. And a rising edge on PA0 doesn't do anything to get me out of this.

    What additional setup do I need to do to get into standby?

    My system only uses two interrupts (USART and Timer, both at priority 0 -- is this a problem?)

    Thanks

    bruce
    bruceAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:44

    I believe I've boiled this down to a problem with my GCC toolchain.

    See my more recent post where I show that it works fine using IAR4.42, but not GCC 4.2.0.