Question
How to get 4 channel input capture values from stm32f407 ?
uint32_t IC2Value,Frequency,miliseconds;
float DutyCycle;
static void TIM2_Config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
TIM_ICInitTypeDef TIM_ICInitStructure;
/* TIM2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
/* GPIOB clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); //Change here, to GPIOA
/* TIM2 chennel2 configuration : PA1 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1| GPIO_Pin_2 | GPIO_Pin_3 ; //Change here, to pin 10
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOA, &GPIO_InitStructure); //Change to GPIOA
/* Connect TIM pin to AF2 */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_TIM2); //And change to pin 1
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_TIM2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_TIM2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_TIM2);
/* Enable the TIM2 global Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* ---------------------------------------------------------------------------
TIM2 configuration: PWM Input mode
The external signal is connected to TIM2 CH2 pin (PB.03)
TIM2 CCR2 is used to compute the frequency value
TIM2 CCR1 is used to compute the duty cycle value
In this example TIM2 input clock (TIM2CLK) is set to APB1 clock (PCLK1), since
APB1 prescaler is set to 1.
TIM2CLK = PCLK1 = HCLK = SystemCoreClock
External Signal Frequency = SystemCoreClock / TIM2_CCR2 in Hz.
External Signal DutyCycle = (TIM2_CCR1*100)/(TIM2_CCR2) in %.
Note:
SystemCoreClock variable holds HCLK frequency and is defined in system_stm32f0xx.c file.
Each time the core clock (HCLK) changes, user had to call SystemCoreClockUpdate()
function to update SystemCoreClock variable value. Otherwise, any configuration
based on this variable will be incorrect.
--------------------------------------------------------------------------- */
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0x0;
TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;
TIM_ICInit(TIM2,&TIM_ICInitStructure);
TIM_PWMIConfig(TIM2, &TIM_ICInitStructure);
/* Select the TIM2 Input Trigger: TI2FP2 */
TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2);
/* Select the slave Mode: Reset Mode */
TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset);
TIM_SelectMasterSlaveMode(TIM2,TIM_MasterSlaveMode_Enable);
/* TIM enable counter */
TIM_Cmd(TIM2, ENABLE);
/* Enable the CC2 Interrupt Request */
TIM_ITConfig(TIM2, TIM_IT_CC2, ENABLE);
}
//And the Interrupt code: //I have changed nothing in it
void TIM2_IRQHandler(void)
{
/* Clear TIM2 Capture compare interrupt pending bit */
TIM_ClearITPendingBit(TIM2, TIM_IT_CC2);
/* Get the Input Capture value */
IC2Value = TIM_GetCapture2(TIM2);
if (IC2Value != 0)
{
/* Duty cycle computation */
DutyCycle = (float)(TIM_GetCapture1(TIM2) * 100) / IC2Value;
/* Frequency computation */
Frequency = SystemCoreClock / IC2Value;
miliseconds = DutyCycle*200;
}
else
{
DutyCycle = 0;
Frequency = 0;
}
}
int main()
{
TIM2_Config();
while(1){
TIM2_IRQHandler();
}
}
I'm trying to get frequency and duty cycle values from input capture mode.It is working for 1 channel but I need 4 channel. So how can I get 4 channel input capture values from stm32f407 ?
Here is my code which works properly: