Skip to main content
SWenn.1
Senior III
November 9, 2021
Solved

How to for loop question??

I have what I am sure to most a simple C question (I'm a hardware guy at this end).....

For brevity I would like to take the following statements and combine them using 1 for loop but don't know the semantics on how to do this....I am using the HAL library with CubeMX:

		TIM2->CCR1 = pwmPulse[speed] - HAPTIC_PW;
		TIM2->CCR2 = pwmPulse[speed] - HAPTIC_PW;
		TIM2->CCR3 = pwmPulse[speed] - HAPTIC_PW;
		TIM2->CCR4 = pwmPulse[speed] - HAPTIC_PW;

Below is a FAILED attempt:

		for (uint8_t i = 0; i < 4; i++)
		{
			TIM2->(CCR1 + i) = pwmPulse[speed] - HAPTIC_PW;
		}

Thanks for the help

This topic has been closed for replies.
SWenn.1
SWenn.1Best answer
Senior III
November 9, 2021

Thanks everyone for the input. I have the following code and it seems to work. Can someone explain to me why (4*i) does not work? The registers are defined as __IO uint32_t, I would have thought that I would need to advance the pointer by 4*i to update the correct register but that does not seem to be the case???

		pTim1 = &TIM1->CCR1;
		pTim2 = &TIM2->CCR1;
		for (uint8_t i = 0; i < 4; i++)
		{
			*(pTim1 + (i)) = (pwmPulse[speed] - HAPTIC_PW);
			*(pTim2 + (i)) = (pwmPulse[speed] - HAPTIC_PW);
 }

6 replies

TDK
November 9, 2021

The only reason this works is because the registers are located consecutively, but you could do something like this:

volatile uint32_t * CCR = &TIM2->CCR1;
 
for (int i = 0; i < 4; ++i) {
 CCR[i] = ...;
}

To avoid confusion, however, and because there are exactly 4 channels, I would recommend not making it into a loop and keeping the original syntax.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
November 9, 2021

The 8-bit count isn't efficient, the natural size for things is 32-bit, and they will be optimal even over small ranges.

The CCR registers are 32-bit wide from the address decode perspective

This is still ugly, but viable

TIM2->(CCR1 + (4 * i)) = pwmPulse[speed] - HAPTIC_PW;

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal
November 9, 2021

Or use a const lookup table containing the addresses, maybe even NULL terminated like C strings.... then you can scatter your pwms in multiple timers if their number grows....

waclawek.jan
Super User
November 9, 2021

For a single timer, if this to be a repeated operation, you could use the mechanism provided by TIMx_DMAR "register". Contrary to its name and description, it is not bound specifically to DMA. Caveat, you must not read it (including through debugger) outside the intended process to not lose track of currently pointed register.

JW

SWenn.1
SWenn.1AuthorBest answer
Senior III
November 9, 2021

Thanks everyone for the input. I have the following code and it seems to work. Can someone explain to me why (4*i) does not work? The registers are defined as __IO uint32_t, I would have thought that I would need to advance the pointer by 4*i to update the correct register but that does not seem to be the case???

		pTim1 = &TIM1->CCR1;
		pTim2 = &TIM2->CCR1;
		for (uint8_t i = 0; i < 4; i++)
		{
			*(pTim1 + (i)) = (pwmPulse[speed] - HAPTIC_PW);
			*(pTim2 + (i)) = (pwmPulse[speed] - HAPTIC_PW);
 }

TDK
November 9, 2021

> Can someone explain to me why (4*i) does not work?

Pointers advance by the size of the thing they're pointing to.

"If you feel a post has answered your question, please click ""Accept as Solution""."