Question
how to flash via dual boot option on stm32l476rg while using mbed os-version 5.x?
Hello,
I am wanting to do flash via dual boot option on a STM32L476RG board using an external board NUCLEO- L476. when I am trying to change the option bit via program in which i am using HAL_FLASHEx_OBGetConfig and HAL_FLASHEx_OBProgram in our main program so that we change the value option byte.but it wouldn't work any more. and please provide me solution in swapping the SRAM1 and SRAM2. if any api is there so that we can able to do this.
Can someone guide me on how I might fix this problem?
Thanks & Regard
Nikhil Singh Gaur