Skip to main content
Furkan2
Associate II
September 26, 2025
Solved

How to filter more than 16 CAN IDs in STM32U5 FDCAN hardware filters?

Hello,

I am working on STM32U5G7VJT6 with FDCAN1 peripheral.
In CubeMX I configured 8 Extended Filters, and in my code I set them as dual filters. That gives me a total of 16 CAN IDs that can be allowed by hardware.

Now my application requires filtering of around 50 unique Extended IDs. Since the hardware allows only 8 filters (dual = 16 IDs), I am not sure how to configure this efficiently for 50 IDs.

My questions are

  1. Is there a way to extend the number of hardware filters beyond 8 (e.g., using extended, or any advanced setting)?

  2. If not, what is the recommended approach for applications needing more than 16 IDs? Should I:

    • Use a broader mask in hardware filters (to accept a group of IDs), and then filter the exact IDs in software?

    • Or is there another technique for optimizing FDCAN filters for larger ID sets?

Any suggestions or example implementations would be really helpful.

Thanks in advance!

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 26, 2025

Hello,

First, in next time please don't post screenshots for your code, but copy paste it in the discussion using </> button.

Second, try to find a common bits having the same values between these IDs and group them using Mask ID filter to simplify the filtering config. That will decrease considerably the number of filters used.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 26, 2025

Hello,

First, in next time please don't post screenshots for your code, but copy paste it in the discussion using </> button.

Second, try to find a common bits having the same values between these IDs and group them using Mask ID filter to simplify the filtering config. That will decrease considerably the number of filters used.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.