Question
how to enable Clock-out capability (MCO Pin)
Posted on May 06, 2015 at 13:00
I want to have a sample of system clock at MCO pin of STM32F107RC micro controller.
I use dspin firmware library for driving stepper motor. The on board crystal is 8MHz and system clock set to be 72MHz. I add this code to ''dspin.c'': GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); and I add the below line code in ''SetSysClockTo72()'' function at ''system_stm32f10x.c'' file. RCC->CFGR &= (uint32_t)0xF6FFFFFF; //HSE clock selected as MCO source But I don't have no clock output on this pin. please guide me thanks yasamin