Skip to main content
sridhar_mo
Associate
September 24, 2009
Question

how to download redboot to STM32?

  • September 24, 2009
  • 3 replies
  • 858 views
Posted on September 24, 2009 at 17:37

how to download redboot to STM32?

    This topic has been closed for replies.

    3 replies

    tomas23
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:23

    Any JTAG tool available, you should use them. Btw. the protocol is described in AN, you can create such tool yourself - I did for STM8 within one day...

    sridhar_mo
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:23

    Hi everybody,

    I am trying to load redboot.bin to STM32 flash through FlashLoaderdemonstrator.exe but I am using Linux PC as host, I tried wine(tools supports to run windows application on linux) but I am getting problem with that tool.

    1) Is there Linux version FlashLoaddemonstrator is available?

    2)If not are there any other ways through which I can download to flash?Please suggest me,If you have some idea.

    thanks

    sridahr

    sridhar_mo
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:23

    I am using ecos env ,STM32 board.

    1)I try to download the redboot.elf to system RAM instead of flash. does it work? or always should be loaded to flash?

    2) I download Flash load demonstrator.exe the host PC is linux, I tried to install wine software(which will allow to run executable) but didn't work out.

    Is there way to load .bin or .elf to load STM32?

    thanks

    sridhar