Skip to main content
Associate III
December 13, 2023
Solved

How to do ADC -> DMA in double buffer mode configuration

Hi All,

I am trying to implement a code on STM32H723 Nucleo-144 where the ADC uses DMA configured in double buffer mode. I cant find any examples on how to do it. I have tried to analyze the ADC to DMA in circular mode code, but I struggle to convert it to double buffer mode. The option to use DMA in double buffer mode doesnt exist in the .ioc file as of my knowledge. Anyone who knows how to do it?

 

I am not an expert on this, so please be patient with me :)

Best regards! 

This topic has been closed for replies.
MasterT
MasterTBest answer
Lead II
December 13, 2023

Certainly, copy data should be faster than ADC 5 MHz conversion clock, can say for sure.

9 replies

MasterT
Lead II
December 13, 2023

Seems it's not written yet, don't see in HAL driver package.

Last time I created double buffer dma-spi function for H743 just to have 32k, other-ways  using Half Complete and Transfer Complete you can get only 16k samples.  There is no more any advantage except overcome dma 16-bits counter limits, so it doesn't worse a trouble. If memory size allows, easy way to have double buffer in software, using common HT & TC interrupts to accumulate a big buffer >32k  of samples by small chunks.

For educational purposes look into HAL, there is:

HAL_StatusTypeDef HAL_DMAEx_MultiBufferStart(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t SecondMemAddress, uint32_t DataLength);

elsoAuthor
Associate III
December 13, 2023

The reason I need it is due to the 16-bits counter limit :)

I want it to work as a ping-pong buffer for MDMA. Tried doing a SW trigger of the DMA Ping pong buffer, but was too slow.

MasterT
Lead II
December 13, 2023

What do you mean "too slow" - having adc running at 5 Msps, 16k accumulated in 3.28 milliseconds - eternity in uCPU word.

Piranha
Principal III
December 13, 2023

Guys, check your math... 2^16 is 64k, not 32k.

In double-buffer mode the address of the inactive buffer can be modified on-the-fly. That way you can swap (rotate) any number of 64k sample sized blocks and don't need any copying at all.

MasterT
Lead II
December 13, 2023

Good catch, the problem only I needed  65536 samples exact for FFT,  and it's not working. So instead of 65k - 1, I downgraded array to 32768 sharp, to keep my perfectionism happy.

 Anyway, OP wants 200k, so software "multibuffer" is only option left.

 Strange things to keep 16-bits register since F1, when new uCPU's have a lot of memory and 32-bits dma CNTR is necessary

Piranha
Principal III
December 15, 2023

Not only the DMA counters should be 32-bit, but also all timers and GPIO ports should have been 32-bit since the beginning. And a normal interrupts for all pins in every port, not the current limited selection of pins through the EXTI.