Skip to main content
Associate III
May 9, 2024
Question

how to create one project and create bootloader and application respectively using compile option

There are a bootloader project and an application project to operate the device.
I am using it by compiling the bootloader project and creating a bootloader file.
I am using it by compiling the application project and creating an application file.


Currently, these two projects are using the same .ioc file.

The main.c file is used differently in the bootloader project and the application project.

 

I would like to know how to create one project and create bootloader and application respectively according to compilation options.

Below is the address area used by the bootloader and application software.

1. Bootloader software
1) FLASH Start address: 0x0800 0000, End address: 0x081f ffff
2) RAM Start address: 0x2000 0000, End address: 0x2002 ffff


2.Application software
1) FLASH Start address: 0x0802 0000, End address: 0x081f ffff
2) RAM Start address: 0x2000 0000, End address: 0x2002 ffff

This topic has been closed for replies.

6 replies

Radosław
Associate II
May 10, 2024

I'm strongly advise against creating one project for bootlader and aplication. I same reason one *ioc. isn't recomended.

Only nested project can bond them together.

 

 

 

 

 

 

Tesla DeLorean
Guru
May 10, 2024

In Keil there's a Multi Project Workspace, can select different subset of files, options, include paths, defines, etc.

 

Whilst I can see some appeal, loaders usually iterate at much slower rates than applications

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
joseph05Author
Associate III
May 16, 2024

I would like to know if there is a way to separately configure the bootloader function and application function code in the main.c file in one project in STM32CubeIDE and build it according to the purpose using compilation options.

Radosław
Associate II
May 17, 2024

Explain why You wanna do this?

joseph05Author
Associate III
May 18, 2024

I have to do a static analysis of the software used in the project, but if there are two project as it is now, I have to do static analysis of both. These two projects have a lot of common software, so things overlap, so if make them into one project, I can do a static analysis only for one project.