Skip to main content
Niyathi Shenoy
Associate III
November 9, 2018
Question

How to continuously store data into SD card?

  • November 9, 2018
  • 2 replies
  • 957 views

I have SD card interfaced with stm32f407 through 4bit SDIO. I am writing data from I2S _DMA_receive buffer into the sd card. This write should happen continuously,but it happens only once.Here is the piece of the code:

FATFS myFATAFS;

FATFS *myFATAFS1;

FIL myFILE;

UINT testByte;

FRESULT res;

uint16_t i2s_rcvbf[2];

uint32_t i2s_final;

while(1)

{

HAL_I2S_Receive_DMA(&hi2s2,i2s_rcvbf,2);

i2s_final= (i2s_rcvbf[0]<<16)+ i2s_rcvbf[1];

HAL_Delay(500);

if(f_mount(&myFATAFS,SD_Path,1)==FR_OK)

{

char myPath[]="0:rec.wav"; 

if(f_open(&myFILE,myPath,FA_WRITE | FA_OPEN_ALWAYS)== FR_OK)

{

HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_14);

if(f_write(&myFILE,(void*)&i2s_final,sizeof(i2s_final),&testByte)==FR_OK)

{

HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_15);

}

f_close(&myFILE);

i2s_final=0x00000000;

HAL_Delay(1000);

}

}

}

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    November 9, 2018

    Writing 4 byte into a file you keep creating doesn't seem like a winning strategy.

    Would also imagine the I2C is choking with an overflow at every iteration.

    Move the mount and file creation out side the loop. Write much more data in each iteration. Try at least 8KB. You might also need to use two buffers, allowing the I2C to fill one while writing the other.​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Niyathi Shenoy
    Associate III
    November 9, 2018

    Hi Clive,

    Thank you for your response.

    I have moved the mount and file creation outside the loop. How to write more data in each iteration? And could you please explain using of two buffers and how to do that?

    My code now is:

    FATFS myFATAFS;

    FATFS *myFATAFS1;

    FIL myFILE;

    UINT testByte;

    FRESULT res;

    uint16_t i2s_rcvbf[2];

    uint32_t i2s_final;

    if(f_mount(&myFATAFS,SD_Path,1)==FR_OK)

    {

    char myPath[]="0:rec.wav"; 

    if(f_open(&myFILE,myPath,FA_WRITE | FA_OPEN_ALWAYS)== FR_OK)

    {

    HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_14);

     }

    }

    while(1)

    {

    HAL_I2S_Receive_DMA(&hi2s2,i2s_rcvbf,2);

    i2s_final= (i2s_rcvbf[0]<<16)+ i2s_rcvbf[1];

    HAL_Delay(500);

    if(f_write(&myFILE,(void*)&i2s_final,sizeof(i2s_final),&testByte)==FR_OK)

    {

    HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_15);

    }

    f_close(&myFILE);

    i2s_final=0x00000000;

    HAL_Delay(1000);

    }