Skip to main content
elmzaiti youssef
Associate III
June 22, 2017
Question

How to configure the DFU ( bootloader USB ) on stm32f7 ?

  • June 22, 2017
  • 2 replies
  • 1085 views
Posted on June 22, 2017 at 09:07

hello , 

      How to configure the DFU ( bootloader USB ) on stm32f7  ? 

    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    June 22, 2017
    Posted on June 22, 2017 at 10:41

    Hi

    youssef.elmzaiti

    ,

    I recommend you to have alook to :

    Please refer to UM0412,

    http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stsw-stm32html

    USB device firmware upgrade STMicroelectronics extension for more details

    on the driver installation and PC host user interface.

    -Nesrine-

    elmzaiti youssef
    Associate III
    June 22, 2017
    Posted on June 22, 2017 at 15:16

    Hi Nisrina 

    we want to migrate from stm32f4xx to stm32f7xx , so this program bootloader DFU on stm32f4xx , it's works , and no on stm32f7xx 

    void bootloader_DFU_400(void )

    {

    /* La fonction est compilée uniquement si on est sur un micro STM32F4xx */

    typedef void (*pFunction)(void);

    pFunction Jump_To_Application;

    vu32 JumpAddress;

    GPIO_InitTypeDef GPIO_InitStructure;

    vu8 bouton_DFU;

    /* Activation Clock GPIO_BP_DFU */

    RCC_AHB1PeriphClockCmd( RCC_GPIO_BP_DFU, ENABLE );

    /* Configuration de PE3 en entrée */

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_InitStructure.GPIO_Pin = PIN_BP_DFU;

    GPIO_Init( GPIO_BP_DFU, &GPIO_InitStructure );

    /*

    Lecture de l'état du bouton DFU

    0 : Bouton DFU appuyé

    1 : Bouton DFU relaché

    */

    bouton_DFU = GPIO_ReadInputDataBit( GPIO_BP_DFU, PIN_BP_DFU );

    /* Si le bouton est appuyé (bouton_DFU = 0) on lance le programme du DFU */

    if ( bouton_DFU == 0x00 )

    {

    JumpAddress = *(vu32*) (ADRESSE_FLASH_DFU + 4);

    Jump_To_Application = (pFunction) JumpAddress;

    RCC->APB2ENR = 0x00004000; //ChL 15/04/2016 besoin de ces 2 lignes pour les micros serie F42x et supérieurs

    SYSCFG->MEMRMP = 0x00000001; //ChL 15/04/2016 besoin de ces 2 lignes pour les micros serie F42x et supérieurs

    /* Initialize user application's Stack Pointer */

    __set_MSP(*(vu32*) ADRESSE_FLASH_DFU);

    Jump_To_Application();

    }

    else

    {

    if (((*(vu32*)ApplicationAddress) & 0x2FFE0000 ) == 0x20000000)

    { /* Jump to user application */

    /* Test if user code is programmed starting from address 0x8004000 */

    /* Jump to user application */

    JumpAddress = *(vu32*) (ApplicationAddress + 4);

    Jump_To_Application = (pFunction) JumpAddress;

    /* Initialize user application's Stack Pointer */

    __set_MSP(*(vu32*) ApplicationAddress);

    Jump_To_Application();

    }

    }

    }