Question
How to configure I2C2 module on STM32F217ZG?
I have managed to communicate via I2C1, but when I switch over to I2C2 I always get a "Busy" response state from the MCU.
Please keep in mind that this is the same I2Cx module from the same datasheet which is set up and executed in the same way as I2C1.
The pins I want to use I2C2 on are PF0 and PF1.
Any sort of help or guidance would be appreciated.
Is there anything from the datasheet I might have overlooked?
Thanks in advance.