Skip to main content
ac.2
Associate II
November 14, 2018
Question

How to configure DMA when STM32F469 uses 16 bit SDRM?

  • November 14, 2018
  • 3 replies
  • 838 views

Hi:​

Let me ask you a question.

When use 32 bits of SDRAM in STM469 official routines, DMA is configured as follows:

 /* Configure common DMA parameters */
 dma_handle.Init.Channel = SDRAM_DMAx_CHANNEL;
 dma_handle.Init.Direction = DMA_MEMORY_TO_MEMORY;
 dma_handle.Init.PeriphInc = DMA_PINC_ENABLE;
 dma_handle.Init.MemInc = DMA_MINC_ENABLE;
 
 
 dma_handle.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 dma_handle.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 
 
 dma_handle.Init.Mode = DMA_NORMAL;
 dma_handle.Init.Priority = DMA_PRIORITY_HIGH;
 dma_handle.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 dma_handle.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
 dma_handle.Init.MemBurst = DMA_MBURST_SINGLE;
 dma_handle.Init.PeriphBurst = DMA_PBURST_SINGLE;
 
 dma_handle.Instance = SDRAM_DMAx_STREAM;
 
 /* Associate the DMA handle */
 __HAL_LINKDMA(hsdram, hdma, dma_handle);
 
 /* Deinitialize the stream for new transfer */
 HAL_DMA_DeInit(&dma_handle);
 
 /* Configure the DMA stream */
 HAL_DMA_Init(&dma_handle);

Now I change SDRAM to 16 bit data width. Should DMA also be modified accordingly? If so, how should it be modified in the configuration?

Thank you very much.

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    November 14, 2018

    Why would the DMA width need to change?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ac.2
    ac.2Author
    Associate II
    November 14, 2018

    Because the data width of my product SDRAM is 16 bits. So I wonder if I want to change the data width of SDRAM dam to 16 bits.

    ac.2
    ac.2Author
    Associate II
    November 14, 2018

    Because the data width of my product SDRAM is 16 bits. So I wonder if I want to change the data width of SDRAM dam to 16 bits.