How to Configure 2 USARTs, One Receive Only vs One Transmit Only + RS485 DE
I am using STM32L432KC: USART1_TX+USART1_DE+USART2_RX. Both are LL drivers.
Currently I have to:
- created 2 additional MX projects
- one with USART1_TX+USART1_DE and dummy USART1_RX pin, set to Mode: Asynchronous + but Data Direction: Transmit Only + Hardware Flow Control (RS485) + DMA USART1_TX
- another with USART2_RX and dummy USART2_TX pin, set to Mode: Asynchronous + but Data Direction: Receive Only + DMA USART2_RX
- Generated the codes and copy the LL init codes of USART1 and USART2 to my own project
- remove dummy USART1_RX and dummy USART2_TX init
Nice to see STM32CubeMX supports such configuration in near future.