How to change the frequency of the PWM using potentiometer
Hello guys good day to you. May I ask you if you can share your experience on changing the frequency of a PWM using a pot. I am using a small board with the STM32F103C8 MCU.
I've set TIM2 _CH1 of PA0 as output. I connected a potentiometer to PA2 (ADC1_IN2 ) to vary the frequency. I am using CubeMX to configure the MCU. Here are the other details:
MCU clock set to 48MHz
ADC clock set to 12MHz
TIM2 prescale to 47
TIM2 ARR set to 0 (I am thinking of modifying the htim period line to vary the frequency)
I used the HAL_ADC_ConvCpltCallback to enable the ADC.
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef * hadc)
{
htim2.Init.Period = ADValue/4; //I was thinking I could vary the frequency this way
TIM2 -> CCR1 = (ADValue/8); //Set duty cycle to 50%
}
However I do not see the TIM2_CH1 having output at all. Can you tell me what is wrong and how to correct this? Thank you for your time.