Skip to main content
Osto
Senior
August 14, 2014
Question

How to change the CPU with STMCube

  • August 14, 2014
  • 4 replies
  • 816 views
Posted on August 14, 2014 at 23:09

Hi,

I have a project with STM32F417 and want to change it to SMT32F407.

I cant find any way to change the CPU.

How can I change without enter all information again into STMCube?

Tkans for you help.
    This topic has been closed for replies.

    4 replies

    jwoolston
    Associate III
    August 14, 2014
    Posted on August 14, 2014 at 23:56

    As far as I have been able to figure out, it is not possible, which is quite annoying. Best you can do if you use their selection filter and then pick a package/variation is change to a different variation (like different package, ram, flash, etc).

    Osto
    OstoAuthor
    Senior
    August 15, 2014
    Posted on August 15, 2014 at 12:37

    Hi,

    Yes I would do that but after the CPU is choosed, after exit and restart the STM32Cube, there is no way to change. I see in the projectt setting the STM32F417 but cant change it.

    Right now, I see that I have to enter all information again.

    Do you have any Idea?

    Thanks
    Tesla DeLorean
    Guru
    August 15, 2014
    Posted on August 15, 2014 at 14:12

    Copy the IOC file, and then edit it

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Osto
    OstoAuthor
    Senior
    August 17, 2014
    Posted on August 17, 2014 at 15:09

    Dear Clive,

    Thats a good idea. I looked at the file but I'm afraid that I write something wrong in it and the whole project will be damaged.

    As you see in the level of the STM32Cube, its right now still in change. It could happen that it cant work correctly because of my wrong information then I probably would search days for a phantom error.

    I already retyped it.

    Thanks