Skip to main content
deep_rune
Associate III
December 23, 2020
Question

How to calibrate STM32L412 ADC

  • December 23, 2020
  • 2 replies
  • 1428 views

I have a STM32L412, I am using a 3V external reference but my ADC is not very accurate - it never reaches its full value, even though the voltage present is the same as the external voltage. I want to calibrate the ADC to see if it improves the performance.

The HAL reference states I need to use the HAL_ADCEx_Calibration_Start before the ADC is enabled, so I have used it just before the HAL initialisation, but when I do this my ADC stops working - none of the bits are set in the subsequent initialisation etc. My exact code for the setup is below. What do I need to do to make HAL_ADCEx_Calibration_Start work properly?

int main(void)
{
 SystemClock_Config();
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_I2C2_Init();
 
 HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED);
 
 MX_ADC1_Init();
 MX_TIM1_Init();
 MX_TIM2_Init();
 MX_RNG_Init();
 MX_TIM16_Init();
 
 ADC12_COMMON ->CCR |= 1<<19 | 1 <<17; // set ADC clock options
 ADC1->CR |= 1>>0; // enable ADC

This topic has been closed for replies.

2 replies

TDK
December 23, 2020
"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
January 8, 2021

Hi @deep_rune​ ,

If @TDK​ 's​  answer resolved your issue, please mark his reply as best answer by clicking on "Select as Best".

If you still need help, feel free to ask your question in more detail.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks