Skip to main content
MGami.1
Associate III
Aug 1, 2020 1:05 PM UTC
Solved

How to calibrate ADC value on STM32F413 series micro controllers ? There is so much noise without giving analog signal on analog pin ?

I am getting so much noise on analog pin without connecting any analog signal. I also tried by changing analog pin but still i am getting so much of noise in analog pin. I am calculating analog value for 50 Hz signal.

Is there any way to calibrate STM32F413 micro controllers ?

Is there any mathematical calculation available for calibration of 50 Hz signal or to reduce noise from signal ?

Please help regarding above topic.

Thanks in advance.

This topic has been closed for replies.
TDK
TDKBest answer
Aug 1, 2020 1:48 PM UTC

There's no automatic calibration for the STM32F4 ADC.

Read this for tips to improve accuracy. In general, there is no silver bullet:

https://www.st.com/resource/en/application_note/cd00211314-how-to-get-the-best-adc-accuracy-in-stm32-microcontrollers-stmicroelectronics.pdf

"If you feel a post has answered your question, please click ""Accept as Solution""."

6 replies

TDK
TDKBest answer
Aug 1, 2020 1:48 PM UTC

There's no automatic calibration for the STM32F4 ADC.

Read this for tips to improve accuracy. In general, there is no silver bullet:

https://www.st.com/resource/en/application_note/cd00211314-how-to-get-the-best-adc-accuracy-in-stm32-microcontrollers-stmicroelectronics.pdf

"If you feel a post has answered your question, please click ""Accept as Solution""."
S.Ma
Principal
Aug 1, 2020 2:18 PM UTC

"I am getting so much noise on analog pin without connecting any analog signal" congrats, you have made your first antenna...

RMcCa
Senior II
Aug 1, 2020 2:28 PM UTC

Use a biquad bandpass filter.​

gregstm
Senior II
Aug 1, 2020 2:55 PM UTC

Even a simple RC filter will cut noise considerably to the ADC, but make sure the resistance is fairly low so that the ADC can work properly (check specs). You can even get away with having two RC filters in series if you choose your R values carefully.

MGami.1
MGami.1Author
Associate III
Aug 4, 2020 9:25 AM UTC

hello @Community member​ 

Can i know which value of resister we have to choose? currently We have taken 1 RC filter and in that r = 1K and C = 22nF. Is it ok? And as you said on more RC filter required for noise reduction?

gregstm
Senior II
Aug 5, 2020 1:15 PM UTC

Ideally you would speak to an electronics engineer (or get a copy of the book "Active Filter Cookbook" by Don Lancaster). A low pass filter with R=1K and C=22nF has a corner frequency of over 7KHz. If you want to reduce the noise in a 50 Hz signal you will need a much larger capacitor eg. 1uF will give a corner frequency of 159Hz. If you want to put two RC filters in series, then usually you make the first R value 10 times less than the second R value. So you could try R1=100, C1=10uF, R2=1000, C2=1uF - both having a corner frequency of 159Hz. Increasing the R value will allow you to reduce the C values, but again, be aware of the ADC's requirements - meanwhile - this site looks pretty educational -

http://www.learningaboutelectronics.com/Articles/Low-pass-filter-calculator.php#answer1