Skip to main content
Associate III
September 5, 2025
Solved

How to brust write by using FSMC?

  • September 5, 2025
  • 3 replies
  • 1034 views

I am trying to send data from STM32 to the FPGA by using FSMC.

My goal is to send data as fast as possible so I set FMC clock to be maximum speed and set sram clock cycles to be as low as possibe.

clock.png

FSMC setting.png

I use FPGA internal Logic Analyzer to capture data from FSMC and the result is shown as below.

sram send data.png

code.png

I found that the data was sent one by one instead of burst mode(send data continuously) and the speed was well below requirement... I want to know how to use burst mode in FSMC?(Since I am using an FPGA to receive data so any mode is ok(PSRAM, SRAM, SDRAM, nano flash, etc)) 

This topic has been closed for replies.
Best answer by KDJEM.1

Hello @snkparty1;

 

According the reference manual RM0090 section "36.1 FSMC main features",  the FMSC supports burst mode access to synchronous devices (NOR flash and PSRAM).

 

KDJEM1_0-1758795535339.png

You can select a burst write in STM32CubeMX configuration.

KDJEM1_1-1758795654865.png

Thank you.

Kaouthar

 

3 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
September 25, 2025

Hello @snkparty1;

 

According the reference manual RM0090 section "36.1 FSMC main features",  the FMSC supports burst mode access to synchronous devices (NOR flash and PSRAM).

 

KDJEM1_0-1758795535339.png

You can select a burst write in STM32CubeMX configuration.

KDJEM1_1-1758795654865.png

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
September 25, 2025

Hello @snkparty1 ,

Apart what @KDJEM.1 said, and according to this thread and this thread: "I tried this on an STM32F429 and the test was successful" it seems you solved the issue. Could you please confirm? and provide the solution?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
snkparty1Author
Associate III
September 25, 2025

Sorry, I forgot this topic. Yes, PSRAM has burst mode. I accepted his answer as the solution. Thanks