Skip to main content
Dan4
Associate II
December 14, 2019
Question

How to access the 2KB user option bytes in H7

In the STM32H7 datasheets, page 23 (H750) or 26 (H743) - ST says the device has 2KB user option bytes flash area.

Does anyone have idea if this is a typo? Or how to access this memory?

If it really is there - it has a good potential to be used as config flash, because it seems independently erasable from the main flash sectors.

This topic has been closed for replies.

8 replies

Dan4
Dan4Author
Associate II
December 16, 2019

Thanks @PMath.4, but the problem is that these functions (used in the link) are not available in the flash_ex HAL files for H7, there are no similar defines in e.g. stm32h7??xx.h, and there is nothing in the reference manual explaining how to access these registers.

I would normally expect that the option bytes (as usual) are not directly mapped on the memory bus but are indirectly accessed via registers (which technically are again accessed via the memory bus, but this is a just a detail).

loeffel2
Associate III
June 17, 2021

Hi Dan

I am also looking for a possibility to use the 2k user option bytes of the stm32h7 devices. But I am not sure if these so called user options bytes could be freely used or not. Did you figure out how the user options bytes could be accessed and programmed?

Best regards

Raphael

Uwe Bonnes
Chief
June 18, 2021

Are there really 2 k of user option bytes beside the user option bits fr configuration? I do not see it mentioned in the reference manual. I do not find in in the memory map neither.

loeffel2
Associate III
June 18, 2021

Dear Uwe

This is the reason I am confused about the user options topic. The data sheet talks about 2k user options but the ref manual dosen't as you mentioned.

loeffel2
Associate III
June 18, 2021

Thanks for the link and clarification of the topic. I will use the first sector of internal flash bank 2 as a kind of OTP replacement.

DanNew
Associate
June 18, 2021

@loeffel2​ - Unfortunately I have not found a way to use this 2KB area. My contacts in ST were not aware either. It would have been convenient with the Value line devices...