I AM THE LINKER, I NEED PUT UART DMA IN RAM, BECAUSE I AM WRITTING IN FLASH, AND THIS DO TALL BUS WHEN I WRITE IN FLASH IN REAL TIME. I AM USING UART DMA, BUT COMUNICATION NOT IS VERY GOOD.
I AM USING DMA: HAL_UARTEx_ReceiveToIdle_DMA(&huart1,Rx_data,Rx_Buff_size);
I HAVE TOO 3 TIMER INTERRUPT, AND 1 EXTERNT INTERRUP.
/* Initialized data sections into "RAM" Ram type memory */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM AT> FLASH