Skip to main content
YSang.11
Visitor II
January 27, 2020
Question

How many times can Flash memory rewrite of STM32G030C8?

  • January 27, 2020
  • 1 reply
  • 1891 views

..

This topic has been closed for replies.

1 reply

Danish1
Lead III
January 27, 2020

From the stm32g030k6 data sheet, I see in Table 42 that the FLASH memory can endure only Nend = 1000 cycles.

Of course you can only program a bit from 1 to 0; this has to be done in 64-bit blocks.

And then erase it from 0 back to 1, in 2kbyte pages.

That amounts to one cycle.

Because of the asymmetry in program and erase sizes, EEPROM-emulation code typically allocates at least 2 pages of FLASH then stores address-value pairs, so that you can write new values to the same emulated address and read back the most-recently-written value without having to erase the FLASH and waste one cycle on every value change. See (for example) ST application note AN3969 "EEPROM emulation in STM32F40x/STM32F41x microcontrollers"

Hope this helps,

Danish