Solved
How many STM32 timers/channels are required to generate 8 synchronized PWM outputs with 4 PWM feedback inputs?
- 1 reply
- 68 views
Hi STM32 Community,
I am currently selecting an STM32 MCU for a timing-control application and would like some guidance on the required timer architecture.
My requirement is:
- Input trigger: 45 Hz, 50% duty-cycle signal.
- After receiving the trigger, the STM32 should generate 8 PWM outputs with a configurable delay.
- The required trigger-to-output delay is approximately 0–3 µs.
- PWM1–PWM4: 45 Hz, 25% duty cycle
- PWM5–PWM8: 45 Hz, 25% duty cycle
- The 8 outputs need to be synchronized according to the timing sequence shown in the attached diagram.
- In addition, I receive 4 feedback PWM inputs:
- Feedback 1–4: 45 Hz, 25% duty cycle
- These feedback signals need to be measured/captured by the STM32.
My main question is:
What is the recommended STM32 timer architecture for this requirement?
Specifically:
- How many timer peripherals would I need?
- Can I use two timers with 4 PWM channels each to generate the 8 PWM outputs?
- Can a third timer with 4 input-capture channels be used to measure the 4 feedback PWM signals?
- What is the recommended method to achieve the 0–3 µs trigger-to-output delay using hardware timers rather than software delays?
- Are there any STM32 timer limitations or channel/pin-mapping issues I should consider when selecting the MCU?
I would appreciate any recommendations regarding the suitable STM32 timer architecture or specific STM32 devices that would be appropriate for this application.
I have attached the timing diagram for reference.