How HAL_UART_Receive_IT() works?
Hello,
I would like to know exactly how HAL_UART_Receive_IT() API works ...?I am using STM32L432KB controller with Quectel's BG96 module to send AT commands and receive its variable length responses.
A demo code of my work is given below.
uint8_t ATE[] = 'ATE0\r';
char buf[100], ch;
int i=0;
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart){
if(huart->Instance == USART1){buf[i] = ch; // filling 'buf', index by index, by 'ch', which has been received from main()
i++;
HAL_UART_Receive_IT(&huart1, (uint8_t*)&ch, 1);
}
}
int main(){while(1){
i=0;
HAL_UART_Transmit(&huart1,(uint8_t *)ATE, sizeof(ATE),1000); // turn Echo OFF for AT commands
// HAL_UART_Receive(&huart1, (uint8_t*)&buf, sizeof(buf), 1000); // if using this API, I can read the response in 'buf', but it takes 1 sec to receive about10 bytes
// @115200 buad. // except this demo, I can't judge how much bytes I am about to receiveHAL_UART_Receive_IT(&huart1, (uint8_t*)&ch, 1); // receiving one byte and storing it in 'ch'
while(!strstr(buf, 'OK')){ // waiting to get full response of AT command, so that it can be used for ERROR handling
}
}
While following this approach to develop my application I am getting many unpredictable results.
Can you help me to figure out what is wrong in this approach and how can I receive any variable length string in minimal time ?Thank You,Maunik Patel