How G-431B-ESC1 drives CAN & PWM communication?
Hello ST,
I bought a G-431B-ESC1, wish to driven with CAN & PWM, but cannot figure it out .
I red the manual(UM2516) was written:
"The CAN interface is provided with transceiver on board and a termination resistor is provided and manageable by firmware. " (page 13/29)
and the only words mentioned about the "firmware" is on page (18-19):
"3. Generate and upload the firmware code into the STM32G431CB MCU with IDE tool available."
However, it is generated by MCSDK.
Since I have used MCSDK for a while and was awared that MCSDK doesn't support "Generating CAN code nor PWM code", and the code proves I am right.
Is there any "FIRMWARE" or code that aviable for drive the CAN & PWM module?
or my only option is writing my own code to drive the modules?
BR
George